Hi Harshitha,
Harshitha Reddy said: almost all the level translators output logic level at 3.3V is VOH level is 2.3V and VOL level is 0.7Max. which will create issue for 3.3V level
Note the VIH for the LMX device seems to be 1.4V min and up to Vcc. Hence…
Part Number: SN74LVC8T245 Other Parts Discussed in Thread: SN74LXC8T245-Q1 Hi Team,
Customer is using SN74LVC8T245-Q1. The input signal rise time can't achieve the requirement in the datasheet. The input pin has RC filter(100Ω+3.3nF), the RC filter can…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74LVC8T245 Hello, Q1: Can SN74AXC8T245 be used for Hot Swap applications? Q2: Can SN74LVC8T245 be used for Hot Swap applications? Q3: Can SN74AXC8T245 be used for Hot Swap applications? …
Part Number: TXU0104-Q1 Other Parts Discussed in Thread: SN74LVC8T245-EP Hello,
I am looking for a 60MHz 1.8V LVCMOS to 5V logic level shifter (4.5V Vih). None of TI's space-qualified logic family seems to be able to do this, as they all operate in 3…
Part Number: SN74LVC8T245 Other Parts Discussed in Thread: SN74LXC8T245 Hello guys,
One of my customers is considering using SN74LVC8T245 with Figure 5 of the device datasheet (Version SCES584B).
https://www.tij.co.jp/jp/lit/ds/symlink/sn74lvc8t245.p…
Part Number: LSF0108-Q1 Other Parts Discussed in Thread: SN74LVC8T245-Q1 , SN74AHC125-Q1 , SN74AHCT125-Q1 Hi team,
i would like to find an automotive qualified voltage translator for below application, would LSF0108-Q1 be suitable here? The SPI data rate…
Part Number: TMS320F28379D Other Parts Discussed in Thread: TPS7A88-Q1 , SN74LVC8T245 , THVD1452 , TPD4E001 , C2000WARE Hi,
We are planning a custom board for BLDC motor drive application.
1. Can we use TPS7A88-Q1 to power TMS320F28379D? Is there any reference…
Part Number: SN74HCS244-Q1 Other Parts Discussed in Thread: SN7404 , SN74LVC8T245 , SN74AHCT541 , SN74AHCT244 Hi,
In a board that I'm designing, I need to "convert" a 3.3V digital signal into a 5V digital signal. So, I think what I need is a non-buffer that…
Part Number: SN74LVC8T245 Hi,
Let me confirm about below.
* Could you please provide ibis model for SN74LVC8T245 or SN74LVC8T245-q1 ?
I confirmed production page, but following URL is not available.
http://www.ti.com/product/SN74LVC8T245/toolssoftwar…