Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74LXC8T245
Dear Specialists
I use SN74LVCC3245A and have a question.
I would be grateful if you could advise.
When VccA = 3.3V, VccB = open, DIR is Low(B toA ), OEn is Low(active…
Part Number: SN74LVCC3245A Hello, My customer has a question for SN74LVCC3245A.
Isn't pin 23(NC) internally connected to anywhere?
They would like to know if they can connect this pin 23 to VCCB(5V).
Regards, Oba
Part Number: SN74LVCC3245A Hi Team,
A couple of our customer's questions about the SN74LVCC3245A:
1. Section 4.10 of the the app note szza036c shows dynamic parameters such as the following:
- Quiet output maximum/minimum - Dynamic level from both…
Part Number: SN74LVCC3245A Hi team,
Where can we get the information of Land size, Resist size and Metal Mask opening for SN74LVCC3245ADB(SSOP(DB)-24)?
Best regards,
Yuto
Part Number: SN74LVC8T245 Other Parts Discussed in Thread: SN74LVCC3245A Hello team,
My customer would like to replace SN74LVCC3245A to the SN74LVC8T245 without modifying PCB.
So, I have searched related threads about termination of 23 pin(VCCB),…
Part Number: SN74LVCC3245A Hi,
SN74LVCC3245APWR states that the absolute maximum rated input voltage Vi is -0.5 to Vcca+0.5V (All A ports).
Is there an allowable value for Vi even if it exceeds -0.5V and +0.5V for pulses within a few ns?
Please…
Part Number: SN74LVCC3245A Dear Specialists,
My customer is considering SN74LVCC3245A and have a question.
I would be grateful if you could advise.
---
We are considering whether we can supply only 3.3V to update the F/W of 3.3V microcontrollers…
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74LVC8T245 Hi,
Customer thinks the following.
On the case of IOL=-24mA, VCCA=2.7V, VCCB=4.5V, VOHB is Min 3.2V.
This means that High output voltage is only increased by 3.2V (Min case…
Part Number: SN74LVCC3245A Hi,
Are there any restrictions on the timing of switching the OE signal (22pin) and DIR signal (2pin)?
Please advise us.
Thanks and best regards, M.HATTORI