Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74LVC8T245 Hi,
My customer has the simple question. According to datasheet, we can not find the recommended land pattern of DB package. Please let us know.
Thanks and best regards, M.HATTORI
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74AHC245 , SN74LVC8T245 , SN74LV126A Hi there-
I'm trying to take a 3.3V microcontroller and communicate with some very old legacy 5V TTL signals. Initially, I was tempted to use the SN74LVCC3245A…
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74LVC8T245 The Absolute Max Ratings include the Input clamp current when going negative, but not in excess of the rail. Is this also 50mA or some lower number.
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74CB3T3245 , SN74LVC245A , , SN74LVC244A Dear expert,
As shown in the datasheet 6.3 section. When VCCA=3.3V and VCCB=5.5V, the high-level voltage VIHB(min)=3.85.
I want do confirm whether B port…
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74LVC8T245 , AVCLVCDIRCNTRL-EVM
Hi all Would you mind if we ask SN74LVCC3245A? Is it possible to use with the condtion VCCA=VCCB=3.3V? We assume that VCCB doesn't have enough tolerance(MIN VCC…
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74LV8151 Hello Team
I am confused the ViH, ViH. My understand is: When the input higher than the 3.85V, the Vo will change to high, when the Input chang from 3.85V to 0.2 V, the Vo will change…
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74AVC8T245-Q1 , SN74LVC8T245-Q1 Team,
Please let me know if a drop-in exists to the 74LVX3245MTR with at least 110C upper temp limit. If there is no drop-in, what is the closest option that has…
Hi
Do you have value of VOHA, VOHB, VOLA and VOLB with the test condition of IOH=-100uA, IOL=100uA at VCCA=2.7V, VCCB=4.5V?
Could you confirm ti?
Bestregards
Other Parts Discussed in Thread: SN74LVCC3245A
Dear Technical Support Team,
I have a question about SN74LVCC3245A.
Do you have a reference value for undershoot if it is beyond datasheet specification?
For example, -0.8V undershoot occurred instantaneously…
Other Parts Discussed in Thread: SN74LVCC3245A Dear Technical Support Team,
I have a question about SN74LVCC3245A.
Do you have a reference value for undershoot if it is beyond datasheet specification?
For example, -0.8V undershoot occurred instantaneously…