Part Number: SN74LVT16244B Hi Team,
our customer is using SN74LVT16244BDGGR. However, they connect one output pin to ground.
Now they want to evaluate the risk of output short.
As I understand, if it output current is less than 50mA, SN74LVT16244BDGGR should…
Part Number: SN74LVT16244B Other Parts Discussed in Thread: STRIKE Hi there,
I see the outputs support hot-insertion, but the datasheet doesn't give more description. In one project, customer uses four pieces of SN74LVT16244B. Only one unit failed after…
Part Number: SN74LVT16244B Hello team,
I have a question on the basic structure of LVT family regarding the ICC, IC's supply current. I checked AVC(Advanced Very-Low-Voltage CMOS) is based on CMOS logic and LVT (Low-Voltage BiCMOS Technology) is based…
Part Number: SN74LVT16244B Hello team,
Could you help me to understand the power consumption of buffer?
My customer is using SN74LVT16244BDGGR, and wants to know how much of power is consumed by this device from power supply's point of view (including…
Part Number: SN74LVT16244B Other Parts Discussed in Thread: TINA-TI Hi Team,
My customer is using the SN74LVT16244B now. The system block is as below.
TP1: green
TP2:blue
TP3: yellow
TP2-TP1: brown
From the waveform and setting, the CPLD output current…
Part Number: SN74LVT16244B Hi team,
We want to check the Hysteresis threshold for the Vih and Vil. For example, if the input higher than 2v, the Vo will be high, when the input drop to which level, the Vo will be low. Thanks.
Part Number: SN74LVT16244B Hello Team,
Can you share the internal input and output circuit structure? Is it push-pull structure? is there pull-up resistors? Thanks.
Regards,
Nanfang
Part Number: SN74LVT16244B Hi, Team:
My customer use SN74LVT16244B and found the input slew rate(14ns/v) is higer than datasheet spec(10ns/v).
They want to confirm:
1. if the 14ns/V is ok or not to SN74LVT16244BDGGR application?
2. why we limit the max…
Part Number: SN74LVT16244B
Hi team,
The customer needs to get the differences for SN74LVT16244BDGGR and 74LVT16244BDGGRG4.
But the electrical parameters and the package are the same from the datasheet for the two devices.
He confuses if the electrical…