Part Number: SN74LVTH162245-EP I have some technical questions regarding 74SN74LVTH162245 that are not covered by the datasheet. The questions are:
1) Can voltage be applied to signal pins 1A1, 1A2, etc. while Vcc is floating? By floating, I mean literally…
Part Number: SN74LVTH16245A Other Parts Discussed in Thread: SN74LVTH162245 Hi Team,
Aside from the 22-Ω series resistors on A-port outputs of SN74LVTH162245, are there other differences with the SN74LVTH16245. Upon checking the datasheets, the two…
Part Number: SN74LVTH162245 Hi,
So i realize NiPdAu plated leads have been around for lots of years however my experience has been mostly in the LEAD processing and really didn't see much issue related to wetting / side fillets.
Currently were running…
Part Number: SN74LVTH162245 Hello Are there any differences among the part numbers SN74LVTH162245DGGR, 74LVTH162245DGGRG4, and 74LVTH162245GRE4?
Also, are those that have the same top markings are the same in form, fit, and function and only differ…
Part Number: SN74LVTH162245-EP Hi , i am relatively new to PCI interface and i am interfacing PCI bus from processor to FPGA. Can i use SN74LVTH162245-EP in my PCI data path and control signals?
And can PCI provide control signals for controlling the…
Hello,
- Junction Temperature Max (Tj Max) – This information can be found in the absolute maximum table of the datasheet.
- Typical Power, (Pd typ) – This can be found in the electrical characteristics section of the datasheet.
- Maximum Power …
Part Number: SN74LVTH32245 Other Parts Discussed in Thread: SN74LVTH16245A , SN74LVTH162245 , SN74LVTH573 , SN74LVTH16373 Hello Team,
My customer has been using the the following devices in several projects.
SN74LVTH32245ZKER
SN74LVTH32373ZKER…
The SN74LVT543 was released with the Bus Hold feature.
The name should have been LVTH543.
In 1997, we issued PCN 5287A informing customers of the name change with a redesign.
In 1999, we issued PCN 5322A notified customers of the nomenclature…