Part Number: SN74LXC8T245-Q1 To whom it may concern -
Does the SN74LXC8T245-Q1 have an input slew rate requirement (min and max requirement)? If so, what is the requirement?
Thanks, Brendan
Part Number: SN74LXC8T245 Can we draw 20mA from each channel continuously without thermal issues? We are connecting HFBR-1521Z transmitter to this SN74LXC8T245. How much current can draw safely assuming for long run of 10 years.
The max current for each…
Part Number: SN74LXC8T245-Q1 Other Parts Discussed in Thread: TINA-TI Hello,
in our new design I use SN74LXC8T245QPWRQ1 for voltage translation 3.3V -> 5V. The circuit drives an external component (no design of our own). The external component has parallel…
Part Number: SN74LXC8T245-Q1 Hi experts
I am designing with the CLXC8T245QDGSRQ1 version of this device (VSSOP package).
The existing IBIS model only supports the TSSOP, VHQFN and UQFN package types, not the VSSOP.
Please provide an IBIS model for the…
Part Number: SN74LXC8T245-Q1 Other Parts Discussed in Thread: SN74LXC8T245 ,
Hi all, I would like to seek advice on the best and most straightforward way of verifying the voltage translation functions of a level shifter part on a test backplane PCB design…
Part Number: SN74LXC8T245-Q1 I understand from the datasheet that SN74LXC8T245-Q1 has weak internal pull-downs of 5-MΩ, which set the default direction of the device from B to A and keeps it enabled all the time. But I want the device to be normally disabled…
Part Number: SN74LXC8T245 Is it ok to have nOE and Dir pulled to +5V when in the powered down state ? i.e., before Vcca comes up to 1.8V ? When 1.8V is good then nOE will be pulled below Vt- to take the buffers out of Hi-Z.
I note that the SN74LXC8T245…