Part Number: SN74VMEH22501A Other Parts Discussed in Thread: TPS38700 Tool/software: Hi Everyone,
I am looking for DC-DC converter or a solution to match power-up sequence between Artix-7 FPGA and SN74VMEH22501A with live insertion capability.
Below…
Part Number: SN74VMEH22501A Tool/software: Hi,
We are re-using an existing design that what using these Transceivers for VME bus. The re-use design is not actually using the buffers, but they are to remain in circuit and powered.
In the existing…
Part Number: SN74VMEH22501A Tool/software: Can B-port withstand up to 5 V during output?
This part is 5-V tolerant but the voltage range applied to B-port output in the high/low state is only up to 4.6 V spec in absolute maximum ratings table?
Which…
Part Number: SN74VMEH22501A Tool/software: Hi everyone,
Please help me to find out the logic level of below signals at Transparent Mode.
OE (Output Enable)
DIR (Direction Control)
LE (Latch Enable)
CLKAB .
CLKBA
Also, please suggest…
Part Number: SN74VMEH22501A I set 3A:Open,3B:GND.When I moved it, the IC generated more than 90°C.
Perhaps the 3A terminal became "H" for some reason, and there was a short circuit with the B terminal inside the IC.
Based on this, is it best to connect…
Part Number: SN74VMEH22501A Tool/software: Hi Everyone,
I need some clarification for below image: ( *Power-Up 3-State (PU3S) Circuits in TI Standard Logic Devices )
Query: If i make change the logic of OE as per PU3S then i will impact my transparent…
Part Number: SN74VMEH22501A Tool/software: Hello,
How to calculate the pull-down resistance value for 3A and 3B ports when they are not being used?
Second, i am new for IBIS model. Please help me to use IBIS model of SN74VMEH22501A to read undershoot…
Part Number: SN74VMEH22501A Other Parts Discussed in Thread: SN74LV14A Hi Team,
My customer is using SN74VMEH22501A and SN74LV14A.
He has question to undershoot of VI. The undershoot may be -0.7V in customer's application, which exceeding abs. max…