Part Number: SN75DP126 Other Parts Discussed in Thread: HD3SS214 Hi Team,
Can SN75DP126 support 1:2 DP 1.1 MUX. I see pin define table seems only support one DP output + one HDMI/DVI.
Can it supports both DP output?
Thanks.
Part Number: SN75DP126 Other Parts Discussed in Thread: HD3SS215 Hi All,
Can SN75DP126 have HDMI input and 2 HDMI outputs? Can HDMI signals be input to the DP input terminal?
Also, do you have any HDMI 1:2 multiplexer products?
Best Regards, Ishiwata
Part Number: SN75DP126 Dear TI ,
I am interested to use an DDI output from the intel GPU to a HDMI connector.
However, as I understand DDI is equivalent to DP++, is that right ?
So A DP126, is compatible with HDMI 1.4b, however I cannot find a solution…
Thanks. We have tried different cable and see improvement on one with integrated ferrites. However we are still outside spec on the harmonics and cannot bypass and test without SN75DP126. Do you have any Eval board for the SN75DP126 with USB-C input and…
Part Number: SN75DP126 Hi Team,
I want to find the chip, it has one input and two outputs. The input should be HDMI or LVDS signal, the output need one DP signal and HDMI signal. Do you have any suitable chips to be recommended?
Best Regards,
Gust
Part Number: SN75DP126 Other Parts Discussed in Thread: TS3DV642 , TDP158 , HD3SS214 Hi Team,
The customer is asking that do we have the similar function device as below which can support up to DP 1.4? I think SN75DP126 should be okay, but it only support…
Part Number: SN75DP126 Hi
When entering the OS, when the output is converted to DP, there will be 4K, but on the HDMI only 1080p
1.Now I2C is not set, can I directly use H/W to set different EQ values? How to set?
2.If I2C setting is recommended, what…