Part Number: SN75DP126 Hello
We'd like to design SN75DP126 in NB product which adopt Whiskey lake of intel.
And input signals from processor DDI directly.
May i have reference schematic of host side?
Thanks
Part Number: SN75DP126 Dear Sirs,
My customer will use the SN75DP126 on new product development.
Could you share SN75DP126 reference schematic, PCBA(Gerber) and EVM guide files to us?
BTW, Do you have any data about HDMI/DP bus layout length from DP126…
Part Number: SN75DP126 Dear Sir,
May I Know the SN75DP126 can or not support HDMI CLK freq up to 297MHz?
If it can support, how to use I2C to adjust CLK freq to 297MHz?
Part Number: SN75DP126 Dear Sirs,
The datasheet mentioned that is supporting resolutions greater than 1920 × 1440 and HDTV deep color at 1080P.
May I know that can or not support resolution up to 4K2K@30hz?
Please advise.
Part Number: SN75DP126 Hi Sir
we use SN75DP126 for switch 2 paths (HDMI & Type-C) and GOP set to DP++, but HDMI's resolution can't reach 4K*2K.
Does DP126 includes Type 2 Cable adapter registers?
Part Number: SN75DP126 Hi,
Am planning to use SN75DP126 for DP(1.2) and HDMI(1.4) output. My input is DP++.
Can any one share reference schematic to implement the SN75DP126 design.
Thanks in advance.
BR,
Pramod
Part Number: SN75DP126 Hello,
My customer is planning to use SN75DP126. It's used for a conversion adapter of DisplayPort and HDMI/DVI.
DisplayPort (DP++) is transmitted by Alternate Mode in USB Type-C. Therefore there are no signals of DDC(SCL_SRC…
Part Number: SN75DP126 Dear Sir,
Customer using DP126 with some issue, they need change EN capacitor C391(1uF) to 10nF then DP126 will work fine.
Do you have idea what happen on it?
Thanks, Ian.