Part Number: SN75LVCP600 Other Parts Discussed in Thread: SN75LVPE801 Hello,
Regarding to SN75LVCP600 (1ch)/601(2ch), my customer is asking some question.
(Question)
(1) What is deference to SN75LVCP600/601 between SN75LVPE801/802
These are pin compatible…
Part Number: SN75LVCP600S Hi Sir
Customer use platform is Intel Skylake H. We can’t connection device when we use u20,u22(SN75LVCP600S). If we remove u20,u22. Then we can connect device.
May you have some suggestion can advise us?
Bogey
sn75lvcp600s…
Part Number: SN75LVCP600S Hi
why we test OOB base on F=750MHz ?
I think SATA is 300, 600 MB/s ?
is there any data descirpt the frequncy is 750MHz ?
thanks
Hi,
The best approach to using the SN75LVCP600 is shown in the attached graphic. I would remove the LVCP600 devices which are adjacent to the SATA transmit pins. There is little or no benefit to equalizer placement in this location.
Regards,
Lee
Part Number: SN75LVCP600 Dear E2E support member,
Regarding the SN75LVCP600 (SATA Re-Driver), is there any guideline for mounting the device manually using a soldering iron (Pb-free)? Specially, we would like to know a duration in which we can touch the…
Part Number: SN75LVCP600 Hi team,
I have two questions.
1. SATA signal polarity should be matched with SN75LVCP600 Rx/Tx polarity?
e.g.
SATA + is connected to RX+
SATA - is connected to RX-
2. The datasheet mentions that the device should be placed…