Part Number: SN75LVCP600S Other Parts Discussed in Thread: SN75LVPE801 Hi Team,
For our SN75LVCP600S, the electrical spec below shows the rise and fall time for SATA/SAS 6 Gbps.
Is this also applicable for SATA 3 Gbps?
If not, do we have rise and fall…
Part Number: SN75LVCP600 Zdiff=80-115Ohm,does it mean the differential impedance shall be controlled to 85-115Ohm,including the tolerance of +/-10%?Or the difference impedance can be 85Ohm+/-10%?
Part Number: SN75LVCP600S Hi
We meet same SN75LVCP600S OOB waveforms issue with last E2E post. e2e.ti.com/.../540166.
Do you have solution for this issue?Because OOB as basic function of the SATA interface. If can't pass OOB test,it may cause function…
Part Number: SN75LVCP600S Tool/software: WEBENCH® Design Tools Hello,
I would like to use a detail part number SN75LVCP600S in my project.
The datasheet says that it allows a hot-plug .
Does it mean I can remove the SSD while transfering data?
If so, what…
Part Number: SN75LVCP600S Hi Team,
My customer is using SN75LVCP600S for redriver function, but after many times test, it can not recognize the SATA hard drive every time, and if I short the wire without redriver, it didn't have any of this issue.…
Part Number: SN75LVCP600S Hi there... I'm using the same SATA circuit in a new design as I did on an older design that was fully functional. However, the new hardware attached to the SATA port is not being recognized. I'm wondering if I need a redriver…
Part Number: SN75LVCP600S For simulation purpose I need IBIS model for the part number SN75LVCP600S, But only HSpice model is available for the same.
Can anyone convert HSpice model to IBIS model and provide ?
Part Number: SN75LVCP600S Other Parts Discussed in Thread: DS125BR111 , DS64BR111 , DS125BR820 , DS125BR401A
Dear Technical Support Team,
I have some problems SATA with SN75LVCP600S.
I think these are caused by AutoLPEXIT (30 ~ 40ns) .
・Host COMRESET Transmit…