Hi Nasser-san,
I appreciate your confirmation.
A customer has an additional question: If LTOL has not been tested, on what basis does SN75LVCP601 guarantee a 0°C operating temperature?
Best Regards, Ishiwata
Part Number: SN75LVCP601 HI,Dear all I use SN75LVCP601 and SSD.
I am trying to test the sata compliance test with a combination of SN75LVCP601 and SSD . Now, SSD will not go into test mode and therefore cannot be tested for compliance.
But, I remove SN75L…
Part Number: SN75LVCP601 Hi,
I cannot check the IBIS version from the product page on the web. Is there a way to check which TI products are compatible with IBIS 7.0?
Thanks,
Conor
Part Number: SN75LVCP601 Hi All,
I have a question about the DEx and EQx pins of SN75LVCP601.
The DEx and EQx terminals are connected internally at 2/VCC. When VCC=3.3V, it becomes 1.65V. In the case of NC, the DEx and EQx terminals are 1.65V, so wouldn…
Part Number: SN75LVCP601 Other Parts Discussed in Thread: DS64BR111 I want simulate from SN65LVCP601 to SSD about SATA signal.
Question Q1. Could you please provide IBIS-AMI files about SN65LVCP601.
Q2. Is ADS the correct simulation tool to use? Q3. Where…
Part Number: SN75LVCP601 Hi Expert,
I have 3 questions about SN75LVCP601RTJR, if the VCC of SN75LVCP601RTJR is 3.3V,
1. May I use 1.8V for differential TX RX voltage level?
2. May I use 3.3V for differential TX RX voltage level?
3. Is it have any differential…
Part Number: SN75LVCP601 Hi
The customer's MB used the redriver SN75LVCP601 because the SATA trace was too long. Connected to Inxxx's 530 120GB SATA SSD and Amphenol 1M cable, the SATA SSD could not be recognized randomly during the reboot test.…
Part Number: SN75LVCP601 Hi,
When "quick search" for the SATA3 redriver, the SN75LVCP601 is not a matching part.
If I lower the protocol to SATA2 redriver, the SN75LVCP601 is seen as an option.
https://www.ti.com/interface/pcie-sas-sata/products…
Part Number: SN75LVCP601
Hi Lee,
In the lvcp601_AMI_users_guide.pdf on Page there are waveforms for rx_int and grx_in probes.
Would it be possible You can share waveform at "rx_in" probe location as well. I do not have access to ADS software- I would…