Part Number: SN75LVCP601 Hi
Can yo help to explain what is that mean in datasheet?
1. Does it mean the trace length at lease need 3 inches before input to LVCP601?
2. the cap should place near to LVCP601 or SATA connector or in the middle?
Eric Lo …
Part Number: SN75LVCP601 Greetings,
The IBIS-AMI model set of files seems to be missing the Tx/Rx s4p models, is there a way to generate these for us?
Thanks,
Shalmon
Part Number: SN75LVCP601 Hello,
I am having problem while simulating the HSPICE file of SN75LVCP601 n ADS 2019 Schematic transient simulation. I have used HSPICE compatibility tool of ADS to put all the pins of the component in the schematic and put all…
Part Number: SN75LVCP601 Hi Team,
cusotmer use SN75LVCP601 to do SATA Gen1~Gen3 signal redriver,but now find that the eye of Gen1 signal has not passed, customer measure TP4 point.
0db is more promising,but no adjustable parameter can be found, can make…
Part Number: SN75LVCP601 Greetings,
We'd like to evaluate the above SATA redriver, is there an IBIS-AMI model we could use for simulation?
Thanks,
Shalmon
Part Number: SN75LVCP601 Hi,
I am planning to design in SN75LVCP601 into my project to drive SATA-3 signal.
Prior to design it in, I need to do verify to see if it can meet the signal quality by SI simulation.
I only found hspice model for this part in…
Part Number: SN75LVCP601 Lee,
We redesigned the board with more length on the connections from the DC blocking caps to the chip and added switches for the settings.
We tried it again without any luck.
We mounted the new re-driver board in a M.2 carrier…
Part Number: SN75LVCP601 Hi Sir
Customer use SN75LVCP601 for sata2 but fail in eye pattern test.
EQ1/2 is NC, DEW1/2 is 0, below is the test result for DE1/2 set to 0/-2/-4.
So what is your comment for this?
PS: sata3 is no any problem.
SN75LVCP601RTJR…
Part Number: SN75LVCP601 Hi team,
My customer is considering to use this device as a repeater.
1. Is this device capable of extend eSATA cable longer than 2m?
2. What is the recommended measurement setup for this device?
Regards,
Itoh