Part Number: SN75LVDS83B Other Parts Discussed in Thread: DS90UB948-Q1EVM Tool/software: Hello,
I’m very interested in the solution you mentioned on the TI forum regarding the RGB/LVDS to HDMI conversion.
https://e2e.ti.com/support/interface-group…
Part Number: SN75LVDS83B Hi team,
1. If the 10% to 90% rise or fall time is greater than 3 ns, how is the input timing defined?
2. What will be the impact if the 10% to 90% rise or fall time is greater than 3 ns?
Thanks
Lillian
Part Number: SN75LVDS83B Hi TIer
My customer use SN75LVDS83B and they have screen noise when power on.
Schematic as bellow:
Screen noise is like video. This problem is also related to temperature. When the temperature rises to 40 degrees, such noise…
Part Number: SN75LVDS83B We have received 3 batch of this MPN:SN75LVDS83BZQLR, But two different types of Xray result. is there any PCN to support? or any explanation or function changes on the circle in the middle?
Package Outline in DS used for comparison…
Part Number: SN75LVDS83B Dear team,
Customer use SN75LVDS83B to convert TTL to LVDS for monitor application.
But face to monitor flashing issue.
We have check CLK input is stable 65MHz.
Could you let me know which signal I need to check for this issue…
Part Number: SN75LVDS83B Dear Sir/Madam,
We have a RGB to LVDS project which used TI's transmitter chip.
I would like to know whether I should keep equal length for RGB and LVDS traces.
I did not find such information on data sheet.
Thank you.
Sincerely…
10 cm is not very long. Are there long traces? What is the total length?
In general, you want a common-mode choke with a low-enough differential-mode impedance (< 10 Ω) and a high common-mode impedance (e.g., 1 kΩ) at the signal/noise frequencies. For…
Part Number: SN75LVDS83B Hi, support team
My customer has the questions as follow:
I'm trying your RGB to LVDS IC witih part number sn75lvds83b. When I did check the output clock , it was different with CLKIN. but the datashee told that the CLKIN will…
Part Number: SN75LVDS83B Hi Team
Customer use SN75LVDS83B in RGB to LVDS application.
They use "33R magnetic beads" between Screen cable and SN75LVDS83B.
The current EMC radiation of the customer's product exceeds the standard.
Is there…
Part Number: SN75LVDS83B Hi team,
Customer has meet an issue on SN75LVDS83B.
After power up VDD and SHTDN is tied on VDD, CLKIN pin accept a period of CLK from CPU but no valid data. Then customer found some abnormal pulsers output at Y0M. you can refer…