Part Number: SN75LVPE802 Other Parts Discussed in Thread: DS64BR111 , Hi,
I am designing COM express based solution for industrial application. I am looking for 2channel redriver. I found the part SN75LVPE802RTJR but looking at the interface forum, multiples…
Part Number: SN75LVPE802 Hello team,
I received a question from the customer regarding to the input signal.
Are there any numerical specifications regarding the input signals (pin 1/2, pin 12/11), and if so, what are the specifications on the input side…
Part Number: SN75LVPE802 Hi,
Could you please let us know the Tj range under recommended operating conditions on SN75LVPE802?
Please advise us.
Thanks and best regards, M.HATTORI.
Part Number: SN75LVPE802
Hello team,
I received a request from the customer. Could you provide the S-Parameter or IBIS model of SN75LVPE802?
Regards,
Masa
Part Number: SN75LVPE802 Other Parts Discussed in Thread: HD3SS3212 , Hello team,
I received a question from the customer. Is it possible to use the SN75LVPE802 in combination with the HD3SS3212 as follows?
Connect TXN to pin 1 and TXP to pin 2 of the S…
Part Number: SN75LVPE802 Hello team,
I received questions from the customer.
1 . Sorry for the rudimentary question, but could you please tell me the role of the equalizer in a SATA re-driver?
2 . The customer did not understand the meaning of the wiring…
Part Number: SN75LVPE802 Hi team,
There are two questions about SN75LVPE802
1. What level of DEW2 (pin 6) is recommended to be set when using transfer rate of 3Gbps by SATA? If set to low, what will be the effect on signal function and quality?
2. Is th…
Part Number: SN75LVPE802 Hi,
Please check below 2 questions.
1. Is Threshold detector and squelch timer in below block same as OOB?
This is redriver block diagram from Intel.
2. V(OOB) Input OOB threshold is OOB entry threshold?
3. What does OOB differential…