Other Parts Discussed in Thread: SPRC121 Hie
I'm looking for an assembly-optimized fft for my c6713 dsp but I'm quite surpised to see that Texas proposes this for :
c64x Little endian
c64x Big Endian
c67x Little Endian
Why there is no c67x…
Hi,
Thanks for your post.
sprc900 , sprc265 and sprc121 are all DSP libraries which are optimized for specific DSP architecture.
sprc900 is floating point DSP software libraries that can be used on any C674x and later platforms.
sprc265 is a fixed point…
Other Parts Discussed in Thread: SPRC121 , TMS320C6748 6711 DSK with ccs 2.00 version.
First strange is, that product install just C6000 dsplib. C6700 dsplib not installed even if sale with 6711 DSK and 6711 DSK connected. Looks like 6700 (floating point…
Hi Venkatesh,
What processor are you using ?
Please refer to the following TI wikis related to DSPLIB
http://processors.wiki.ti.com/index.php/MexExample http://www.ti.com/tool/sprc121 http://www.ti.com/tool/sprc265 http://processors.wiki.ti.com/index.php…
Hi,
Thanks for your post.
To do simple filtering on DSP processor, please download the TI C67x DSPLIB from the below link in which you could see filtering and convolution libaray functions:
http://www.ti.com/tool/sprc121
For C674x device, please check…
Hi Rakesh,
Thanks for your post.
These are functions that exist in libraries supplied by TI or the DSK board vendor. Your project must include these libraries to be able to use these functions. So, please download the TI C67x DSPLIB from the below lin…
Hi Yimin, My customer is using the following DSPLIB. http://www.ti.com/tool/sprc121 This is for c67x core and they are using this on C6713. Now I'm trying to get the source code to reproduce the issue. Once I confirm the issue at my side, I'll be back…
Hi,
I think, you can very well integrate the DSP libraries & appropriate include header files in the starterware (non-OS) project which would be more convenient to start working with. For this to work in the starter ware audio loopback project, you must…
Hi,
Thanks for your update.
If this is the case, please download the TI C67x DSPLIB from the below link in which you could see filtering and convolution libaray functions:
http://www.ti.com/tool/sprc121
For C674x device, please check the supported kernel…
Hi Eric,
Thanks for your post.
To my knowledge, the AIC3106 codec performs with 20-kHz low-pass filter which removes out-of-band noise and it is obvious that the low pass filter is enabled by default with specified passband & stop band. So, it is not…