Hi Chris Magner,
Download the package, "sprc234.zip" which contains the SRIO code at "..\C645x\sprc234\03.00.10.02\6455\6455_default_package\default_package\csl_c6455\example\srio"
For 6455, with reference to the TRM, please refer…
Other Parts Discussed in Thread: TMS320C6455 Hi Folks,
I have downloaded the CSL from the below link for C6455.
http://www.ti.com/tool/sprc234
Does CSL has support for C6455 PCI module ?
Thanks,
Srijan
Other Parts Discussed in Thread: SPRC234 , CCSTUDIO Hi, I have CC v3.3 project, and now I need port it to CC V6.
My project need BIOS and CSL
1 I setup Version: 6.1.0.00104 have RTSC/XDCtools 3.31.00.24 and setup bios 6.41.2.41 is it ok or need use other…
I'm sorry. The UART Code was written by the The TMS320C620x C642x McBSP UART ( spra633c ) . McBSP-EDMA3 Interrupt refer to the C6455 Chip Support Libraries ( sprc234 ) code . Two files will be attached .
0268.uart.c
/****************************…
Hi,
Please validate your configuration with the TI's SRIO CSL example. You can find the SRIO master/slave project at the BSL package for C6455. This example demonstrates two way communication between two DSPs connected through a 4 lane, point to point…
Hi Maxim,
In general, if you would like to know "How to set and use interrupts for TMS320C6x DSP", it is worth starting from this generic document http://www.ti.com/lit/an/spha001/spha001.pdf and then move on.
In addition to that, the interrupt controller…
Hi,
Sorry for the delayed response,
I could not find any test code for HPI interface for OMAPL138 device,
http://www.ti.com/lit/ug/spru578c/spru578c.pdf
But, I found HPI test code for C6455 device,
Please take this code as a reference and modify it for…
Hi,
Thanks for your post.
Is it your TI provided code or your own custom code?
I think, there is an app. report on the EMAC controller software operation on c645x DSP as below:
http://www.ti.com/lit/an/spraa90/spraa90.pdf
Please refer section 7.4 in which…
Other Parts Discussed in Thread: SPRC234 I am investigating porting a DSP/BIOS 5 project to SYS/BIOS 6. I think I have resolved all bar one of the compiler issues but cannot see a 'clean' solution to the fact that XTC's std.h contains:
typedef…