Hi Jeong Sng,
Is this Source code supplied by TI ? If yes, Do you modify the supplied code for your project requirment? Would you please mention the details like name of the CSL package and version e.t.c
Did you uncover the code errors in the CSL package…
Hi Ricky,
How can I improve the performance of EDMA3?
I am not expert on EDMA3 but I will give you some hints on this.
Please refer the following TI wiki to increase the throughput of EDMA3
This is not exactly for C6455 but It talks about typical EDMA3…
Other Parts Discussed in Thread: CCSTUDIO , SPRC234 , TMS320C6455 RandyP, I ported the dks_app example for the Spectrum Digital C6455 evaluation board into CCS5.5.0 and was (finally) able to get the code to compile, link and run--almost. I can see the visual…
Lisa,
Thanks for staying with me on this. Although the DOS window gives me a work-around, I loose an awful lot of the benefits of the IDE, so I still really need to sort this out.
I ran the makefile from the directory CCS put it, i.e. couple levels …
Other Parts Discussed in Thread: TMS320C6455 , SPRC234 , CCSTUDIO Greetings
It seems that the CSL_DEV_REGS in the soc.h header file is incorrect. It reads 0x02A8000 0 instead of 0x02A8000 8 . Details are as follows:
- I'm using CCS 3.3.38.2 (Code Generation…
Hi Jason,
Probably you are not using the correct CSL for C6455.
You can refer to the following thread for the similar problem:
http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/6629/25306.aspx#25306
And the CSL package for C6455…
Other Parts Discussed in Thread: SPRC234 Hello friends!
I am using sprc234 Chip Support Library for 6455, version 03.00.10.02; call CSL_sysInit() as described in its document. But csl_c6455.lib does not contain this function. Evenmore, there is no CSL…
Manuel,
I don't have any examples that configure interrupts using only basic register access, but there are several examples showing how to configure interrupts using CSL. First, download the CSL release for C6455 from this page:
http://focus…
Other Parts Discussed in Thread: SPRC234 The DSP is C6455, I use the EDMA example in SPRC234 with no modification, the project is in default_package\csl_c6455\example\edma\edma_interrupt\build, however, after I run it, the programme always stops at "while…
Hisni,
Which version of the csl are you using? The latest is at:
http://focus.ti.com/docs/toolsw/folders/print/sprc234.html
There is an emifa and a gpio example under the directory default_package\csl_c6455\example\
Besides that, all you should…