Hi Patrick,
nothing is wrong, we found out an unexpected bug in the software. The correct version will be updated by today on the website. In the mean time I can share with you this version in advance. Could you please try it out and check if you face…
Hi Maury,
I was able to reproduce the warning with your project using the TMS320F28377S_NO_APPL.cmd linker command file. I couldn't resolve the problem in your project, so I tried to reproduce it in a smaller, simpler case. I started with the controlSuite…
I am using EVE SW version "eve_sw_01_18_00_00" .
my testcases passes with the image. please find attached input image. PLEASE REMOVE THE .txt EXTENSION BEFORE USING THE IMAGES. I CHANGE THE EXTENSION TO UPLOAD THE FILE BECAUSE FILE IS NOT GETTING UPLOADED…
Hi Brijesh,
I tried with both 8 bit and 16 bit extraction.
The image with 16 bit pixel extraction looks the same which we were getting before( by disabling pixel processing)
The image with 8 bit pixel extraction does not look good.I am attaching…
Hello Danish!
I have 2 news:
1st: Debugging installer behaves the same as others, i.e. after starting I see the same message box about the error.
2nd: I found out the reason of this problem. This is partly my fault. Usually I use by file manager…
I am using Tiva C series TM4C123GXL launchpad to program my target device and debug it. My target device is TM4C123GH6PGEI micro-controller. The kit programs the target occasionally and fails to do program sometimes. Besides the resistance between RESET…
Part Number: CC2642R Our application is based on Simple Peripheral but without any pairing and/or GAP bond manager. While we use Ellisys Bluetooth analyzer heavily for understanding the BLE communication, we are seeing that when we try to connect to the…
David,
Here is the patch for issue #2.
To install the patch:
Make sure the user's CCS version is 5.3.0.00090 - the patch will only work on this build of CCS.
Download the attached file, and change its extension to ".jar".
Find the file with…
Arefeen,
If you run the controlSUITE installer and select the HV Kit the following directory will appear
C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit
with the following directories
\Docs = How to Run Guide (attached)
\HW Development…
Hi Erik,
The patch is attached. It is only applicable to CCS v5.2.1.00018, so please make sure that is the version of CCS that you have (see Help > About... dialog in CCS).
Please install the plugin into your CCS v5.2.1.00018 image as follows:
…