Part Number: TAS2552 Other Parts Discussed in Thread: TAS2555 , , TAS2553 Hi Sirs, Would you pls advise the rise and fall time specification referring to which signal (BCLK, LRCK or DATA?) in the TAS2552/TAS2553/TAS2555 datasheet? There are 4ns specification…
Other Parts Discussed in Thread: TAS2553 We are planning on using the 2.8W TAS2553 for a project which uses a 3.7V battery.
Should VBAT on the amplifier be connected directly to the battery or should it instead be connected to a voltage regulator?
If using…
Nikunj Patel said:
Ans: TAS2553 IC required 22.5 MHz mclk. still, we does have 22.5Mhz on B26 Pin so currently we are using the 1.8Mhz internal Oscillator[also use the PLL] of TAS2553 IC by changing the TAS2553 Configuration. and still not clear audio…
Part Number: TAS2552 Other Parts Discussed in Thread: TAS2553 , , TAS2557 Hi Team,
We want to use smart AMP to improve the audio performance, but our platform only has analog output, no I2S interface, so we can only chose TAS2552 or TAS2553.
As I know,…
Hi Vincenzo,
You can have a look at the following devices: TAS2505 and TAS2553. I think that these devices comply with your requirements.
Best Regards
José Luis Figueroa
Audio Applications Engineer
Hi Ivan,
Thanks for the response. Can you help provide some clarification to the following questions:
1) What is the maximum current that the I2C pins (SCL/SDA) can sink on TAS2552?
2) Is the output HOLD time from TAS2552 0''?
3) Based on #1…
Other Parts Discussed in Thread: TAS2553 , TAS2552
We are planning to use the audio codec TAS2553 in our end design.
We would like to know if you have any EVM available for TAS2553 to be interfaced with i.Mx7 Dual. Please share the full part number of…
Other Parts Discussed in Thread: TAS2553 , LM48511 , TPA2016D2 Hi ,
We are looking for an D class Audio amplifier with Gain control to drive 0.8W / 1 W, 8 ohm Speaker to achieve Sound pressure level of min 80dBA ( 100Hz- 10Khz) with no more than 3% THD+…
Other Parts Discussed in Thread: TAS2553 , TAS2505 Hi,
Currently I am Using TAS2553 in one of my project, I have quesation regarding power on sequence requirement of TAS2553.
As per the datasheet the power on sequence is VBAT-->IOVDD-->AVDD
but in…
Other Parts Discussed in Thread: TPA2038D1 , TAS2553 Hello,
Customer is looking for a low cost, mono, analog in, class D amp that will deliver 3W@1% THD+N, 4 ohm load with a 5 V supply. Adjustabe gain would be nice but not a must. I suggested the TPA2038D1…