Part Number: TAS5754MDCAEVM Other Parts Discussed in Thread: TAS5754M Hi,
I am using PurePath Console ver2.1-rev35934 to dumping TAS5754m register to two .h format files with burst value setting to 1, and another burst value setting to 10.
I did follo…
Part Number: TAS5754MDCAEVM Other Parts Discussed in Thread: TAS5754M Dear Sir,
We tested TAS5754M EVM THD+N performance as below but looks a little bit gap with d/s shows, is it make sense for test result?
PVDD=18V PO=1W INPUT=1KHz LOAD=4ohm (LINE IN…
Part Number: TAS5754MDCAEVM Hi,
I've connected a PPCMB (AIP006G) with a TAS5754EVM, and am attempting to look at the I2S clock and data signals. I'm streaming audio input via USB, and interfacing with the board via PPC2 GUI. The audio is successfully…
Part Number: TAS5754MDCAEVM Other Parts Discussed in Thread: TAS5754M Hi all,
I am facing some issues with the TAS5754MDCAEVM board and the PurePath Console.
I am connecting through the USB port and I manage to open the PurePath Console successfully…
Other Parts Discussed in Thread: TAS5754MDCAEVM
bought the Purepath-CMBEVM + TAS5754MDCAEVM that are constructed as 2.1 using two TAS5754M .
Managed to download Purepath Console 1.16 and the software only have TAS5760 that is 2.0 . According to the TAS5754…
Other Parts Discussed in Thread: PUREPATH-CMBEVM , TAS5754MDCAEVM , TAS5754M I bought the Purepath-CMBEVM + TAS5754MDCAEVM that are contract as 2.1 using two TAS5754M .
Managed to download Purepath Console 1.16 and the software only have TAS5760 that is…
When we designed this TAS5806MEVM, our software team required that the bottom device (U2) could work in both BTL and PBTL. That's why you see the two big 390µF caps on PVDD.
TAS5754MDCAEVM is different. The bottom device on it only works in…
Hello,
in this thread I find some important information: e2e.ti.com/.../701840
Andy Liu SH:
The PPCMB (PurePath Console Mother Board) will detect the FW ID of the attached TAS5756MDACEVM when PPC2 is launched. Your hardware connections are definitely…
No. The FW ID is stored in the EEPROM on the TAS5754MDCAEVM. TAS5754MDCAEVM has to be mounted to PPCMB to make PPC2 work correctly.
I would suggest you guys make your tuning using the TAS5754MDCEVM and PPCMB.
Andy