Part Number: TCA9511A Dear team,
We have I2C and lower speed signal(like wake, PERST, CLK request) in our application, and need hot swap function for this signal.
Can we use TCA9511A on both I2C and lower speed signal?
If not, could you recommend hot…
Part Number: TCA9511A
Hi Team,
If EN is not connected to VCC, but to another power supply, and pull up the output signal (SDA_OUT/SCL_OUT) to the power supply where the EN pin is located, is there any risk in this use? Thanks.
Regards, Charlie
Part Number: TCA9511A Other Parts Discussed in Thread: TCA4307 , TCA9517 , TCA9800 Our product uses an I2C bus from a BeagleBone Black Industrial (BBBI) to communicate with two motor speed controllers (MSC). When a motor speed controller is powered down…
Part Number: TCA4307 Other Parts Discussed in Thread: TCA9511A , Hi,
The TCA4307 and TCA9511A have very similar specs, and as far as I can see are pin-to-pin electrically compatible (contrary to website).
The only difference I can see is that the TCA4307…
Part Number: TCA9511A Other Parts Discussed in Thread: TCA4307 , TCA4311A Hi team,
Customer want to use TCA9511A p2p replace TCA9411A, and want to check with us about the spec difference of those two part, could you help if those two part could be p2p…
Part Number: TCA9511A Hi team,
how cascaded I2C buffers (such as TCA9511) work?
In cascaded case, how can TCA9511 know which side or which direction is driving low?
could you give a detailed discription on how is the bi-direction mechnism work(for a single…
Part Number: TCA9511A Other Parts Discussed in Thread: PCA9306 Hi,
If I power the TCA9511A off a 3.3V rail, can I connect it to a 5V bus? The datasheet suggests tying the bus lines to VCC, but the maximum ratings for those pins is not dependent on VCC…
Other Parts Discussed in Thread: TCA9511A
FAQ: Logic and Voltage Translation > IxC >> What Makes an I2C Buffer Hot-Swappable ?
Hot-Swap also known as Hot-Plug means the unpowered device can be inserted into a live backplane without disruption of service…
Part Number: TCA9511A Other Parts Discussed in Thread: TCA4311A , TCA9617A Hi team,
My customer evaluation TCA9511A and TCA4311A, and have some questions, please help me.
1、9511 and 4311 are hot-swappable chips. What is the main difference between them…
Other Parts Discussed in Thread: TCA9617B , TCA9509 , TCA9801 , TCA9800 , TCA9803 , TCA9802 , TCA9511A , TCA4307 FAQ: Logic and Voltage Translation > IxC >> What Connections of I2C Buffers are not Allowed ?
Part Numbers: TCA9517 , TCA9517A , TCA9509 , TCA9…