Part Number: IO-EXPANDER-EVM Other Parts Discussed in Thread: TCA6416A , TCA9534 , TCA6408A , TCA9535 , TCA6424A Tool/software: Hi,
Customer want to know which IC is on IO-EXPANDER-EVM, as we see the EVM instruction includes lots of chip (TCA6408A, TCA6416A…
Part Number: TCA9534 Other Parts Discussed in Thread: PCA9534 Hi,
Our customer used TCA9534 and need to confirm one question about interrupt, does TCA9534 get multiple interrupt? His application need several external interrupts, and these interrupts could…
Part Number: TCA9534 I am having difficulty communicating with the TCA9534. I am probing the I2C Clock and Data lines. I can see the Master has initiated the Start Condition. I can see that the slave address is clocked out. I can see the Write command…
Part Number: TCA9534A Other Parts Discussed in Thread: TCA9534 , Dear colleague,
Our customer are concerned about the difference between TCA9534A and TCA9534.
I check the datasheet, I don't find the obvious difference.
Best Regards,
Rock Su
Part Number: TCA9534 Hello,
I have assembled a board with a TCA9534 and when I power it with 2.85V the part pulls the supply down to 0.95V. I can confirm that the TCA9534 is the issue because it gets warm to the touch and no other parts are connected…
Part Number: TCA9534 Hi, Sir:
Customer needs definition of Marking.(Like following picture)
Could you help to provide it or Top Side Marking Drawing?
Thank you.
+------------------+
| \\T/ YM | \\T/ =TI
| o VRDQ | YM=Year /Month Date Code
+--…
Part Number: TCA9534 Hello TI Engineers,
I have a service request which customer use extender TCA9534 with Arduino uno through this library.
github.com/.../TCA9534
It seems to work with Arduino well but not working properly with ESP32 wroom.The customer…