Part Number: TCA9534A Other Parts Discussed in Thread: TCA6416A , TCAL6408 , TCA6408A Hii Team,
I'm, planning to use TCA9534A in our project. I want the I2C Interface to work at 3.3 V level but few GPIOs at 3.3 V level & few GPIOs at 1.8 level. Will…
Part Number: TCA9534A Other Parts Discussed in Thread: TMAG5273 , , TCA9543A
Tool/software:
Hello, I am using the TMAG5273 Hall sensor and the 8-channel TCA9534A GPIO expander.
I connected the Hall sensor's interrupt pin to a GPIO pin on the GPIO…
Part Number: TCA9534A Tool/software: Hi Team,
we using GPIO to simulate I2C to control the TCA9534A.
When I send I2C commands, such as I2C get unit 0 dev 14 reg 0x0 , it works fine for the first four command after power on. However, starting from…
Part Number: TCA9534A Tool/software: Hi Sir,
We found Tj (max) only 100 o C in the datasheet, is it correct? Normally the Silicon IC should be 125 o C degree.
If the Tj(max) is only 100 o C , what's the max. power consumption for TCA9534A.
We would…
Part Number: TCA9546A Other Parts Discussed in Thread: USB2ANY , TCA9539 TCA9546A is used with TCA9539, how to use USB2ANY for communication?
TCA9546 A2A1A0 connect to ground salve address0x70, how to understand control register??(need to config channel…
Part Number: TCA9534A Other Parts Discussed in Thread: PCA9534A , Hi Team, aside from the supply voltage we want to further understand the difference between PCA9534A and TCA9534A.
Thank you.
Part Number: TCA9554A Other Parts Discussed in Thread: TCA9534A Hi team,
My customer would like to know what's different between TCA9554A and TCA9534A?
From simple comparison table, I can't judge their difference, so please advise.
Thanks
Part Number: TCA9534A Hello Guys,
Good day.
Our customer need some clarification on the Electrical characteristics P-port voltage. The P-port voltage is lower than VCC on data sheet Page6. e.g. IOH=-8mA VCC 1.65V MIN P-port voltage 1.2V Under what…
Part Number: TCA9534A Other Parts Discussed in Thread: TCA9554A
1) We expected to use IO 0-7 to control LED, which part is suggested by TI?
TCA9534A or TCA9554A
2) Does TI suggest that I/O port connect to LED directly?
3) Check datasheet, TCA9554A…