Part Number: TCAN1043HG-Q1 I have a doubt here:
Once CAN iC enters sleep mode,but if my VIo supply is available for another 50+ mS(Supply Capacitor discharge time) and EN is Hi at that time,does it go to Wake up mode again.
a)Is there any max time within…
Part Number: TCAN1043HG-Q1 Other Parts Discussed in Thread: TCAN1043-Q1 Hi TI experts!
We've noticed different color of leads cross-section and I would like to ask if this has effect on the device performance?
Part Number: TCAN1043HG-Q1 hello Team,
I was looking for a CAN-FD capable Transceiver for automotive applications in ECUs used in 24V board nets and came acrosss the TCAN1043HG-Q1 which looked to me as a perfect match.
However now I got asked, if the…
Part Number: TCAN1043HG-Q1 Other Parts Discussed in Thread: TCAN1043 Dear:
External Connection Description of TCAN1043: INH pin is NC state.
Two operating:
State 1: After power-on, WAKE pulls to high, works for a period of time, and then pulls…
Hi Sikesh,
The NC pin can be left floating or pulled to ground. The datasheet section 9.2 'Typical Application' (page 34) shows the pin left floating. On the TI TCAN1043-Q1 EVM, the pin is default floating with an optional pull-down resistor: …
Part Number: TCAN1043HG-Q1 Other Parts Discussed in Thread: TCAN1043 Hi, I have two question related to fault condition - I have a processor interfaced with transceiver (TCAN1043HGDQ1) and also I have connected microchip CAN analyser on the same bus. 1. Refer…
Hello Eric/Clemens,
Can you please provide any documentation which can describe the all support physical layer requirement for ISO11898 and SAE 2284-4 for TCAN1043HG-Q1?
We got input from end customer that there is some physical layer requirement also…
Part Number: TCAN1043HG-Q1 Hello,
my customer reached out and asked if we could please provide them with the 3D model in STEP format of the TCAN1043HGDMTRQ1 device?
I look forward to your feedback.
Best regards,
Stani