Part Number: TCAN1043HG-Q1 Other Parts Discussed in Thread: TCAN1043 Dear:
External Connection Description of TCAN1043: INH pin is NC state.
Two operating:
State 1: After power-on, WAKE pulls to high, works for a period of time, and then pulls…
Hi Khyati,
Khyati Sapariya said: Does this means that fault will occur only when processor is transmitting data on TXD pin of TCAN1043HGDQ1 and any of the six condition is true?
Yes, TCAN1043 will only detect these fault conditions when it is transmitting…
Hello Eric/Clemens,
Can you please provide any documentation which can describe the all support physical layer requirement for ISO11898 and SAE 2284-4 for TCAN1043HG-Q1?
We got input from end customer that there is some physical layer requirement also…
Hi Sikesh,
The NC pin can be left floating or pulled to ground. The datasheet section 9.2 'Typical Application' (page 34) shows the pin left floating. On the TI TCAN1043-Q1 EVM, the pin is default floating with an optional pull-down resistor: …
Part Number: TCAN1043HG-Q1 Hello,
my customer reached out and asked if we could please provide them with the 3D model in STEP format of the TCAN1043HGDMTRQ1 device?
I look forward to your feedback.
Best regards,
Stani
Part Number: TCAN1043HG-Q1 Other Parts Discussed in Thread: TCAN1043 , TCAN1043H-Q1 Hello Sir, I am looking into Automotive CAN transceivers for our application, I came across TCAN1043HG-Q1, I am not sure why the Vsup is used for.
Thanks Akilan G
Part Number: TCAN1043HG-Q1 Other Parts Discussed in Thread: TCAN1043 Dear team,
cal
There is a calculation for normal speed CAN bus to estimate the max cable length and total stub limitation. If designing CAN FD 2Mbps with TCAN1043, do we have a equation…
Part Number: TCAN1043HG-Q1 Other Parts Discussed in Thread: TCAN1043 Dear TI customer support,
for automotive CAN and CAN-FD applications, we are currently considering two transceivers: TI TCAN1043HG-Q1 and NXP TJA1043. Both are great CAN transceivers…
Part Number: TCAN1043HG-Q1 Team,
The datasheet mentions that the WAKE “terminal triggers a LWU on either a low-to-high or high-to-low transition since it uses a bi-directional input threshold (falling or rising edge)”. In the case we consider a low-to…