Part Number: TCAN1051-Q1 Hello,
My customer was wondering what the absolute maximum ratings for V(logic_input) at VIO=3.3V is because I'm not sure if it is +7V or 3.6V(VIO+0.3V) since the datasheet says +7V and VI=<VIO+0.3V. Would you please tell…
Part Number: TCAN1051-Q1 Hi Team,
We are selected “ TCAN1051DRQ1 ” CAN IC in our design,
TCAN1051DRQ1 IC, VOH min: 4V @ 2mA mentioned in datasheet
MCU , VIH min: 4V , MCU input leakage current is 1uA
For Logic Compatibility Margin is zero for…
Part Number: TCAN1145-Q1 Other Parts Discussed in Thread: TCAN1051-Q1 , Hi expert,
My customer is BTL and for some complicated reasons they want to use the TCAN1145-Q1 to run in only Normal and Silent modes. Similar to TCAN1051-Q1, it has only two modes…
Part Number: TCAN1051-Q1 Other Parts Discussed in Thread: TCAN1044-Q1 Hi.
We are using TCAN1051Q automotive version with silent mode witch disable the transmitter part.
part of the chip characteristic are it's differential input capacitance and resistance…
Part Number: TCAN1051-Q1 Dear support team
My customer use TCAN1051-Q1 and they confirm behavior that CANH/L output is 0V at 85 deg /85% humidity.
Is there any mode that CANH/L output is 0V other than dominant and recessive?
Regars
Tomohiro Nagasawa
Part Number: TCAN1051GV-Q1 Other Parts Discussed in Thread: TCAN1051-Q1 Hi Expert,
My customer is using multiple TCAN1051-Q1 in their design and wants to check what is the correct implementation of the termination resistor?
My understanding is like datasheet…
Part Number: TCAN1051-Q1 Hello,
My customer is wondering if TCAN1051-Q1 works well regardless of the ramp(rise) time even 1ns or 1sec. The datasheet doesn't say anything on it, but they had an issue recently on another IC when the ramp time is too slow…
Part Number: TCAN1051-Q1 Other Parts Discussed in Thread: TCAN1051 , SN74LVC2G14 , SN74LVC2G132 Hi,
Can i get a CAN repeater without any MCU or CPU? Use two TCAN1051 and some logics?
Part Number: TCAN1051-Q1 Other Parts Discussed in Thread: TCAN1051 Hello,
Can TCAN1053-Q1 use alternative device for R2A25416SP? It would be helpful to let us know alternative device if TCAN1053-Q1 is any issue for alternative.
Best regards,
Toshihiro W…