Part Number: TCAN1462V-Q1 Hello team,
I received a question from the customer.
If only VIO is shut off from VCC (5V) and VIO (3.3V) being supplied, does VCC ever affect the VIO line?
Regards,
Masa
Part Number: TCAN1462V-Q1 Hi,
Good Day.
In the datasheet, it is mentioned that the transceiver loop delay is 160 nsec max.
They said the bit rate is less than the loop delay.
Do we have to enable the transceiver delay mechanism for proper working?
The…
Part Number: TCAN1462V-Q1 Hi expert,
Regarding TCAN1462 V -Q1
Does TCAN1462V have any limitation for power up/down sequence between Vcc and Vio?
For example, If customer supply power to Vio only, does Vcc pin have any leakage voltage? (also, how about…
Part Number: TCAN1462-Q1 Other Parts Discussed in Thread: TCAN1462V-Q1 Hi team,
Our customer has been designing with TCAN1044AVDRBRQ1 and now they want to switch to TCAN1462V-Q1(SON8) as SIC becomes required.
I know these two devices are pin to pin compatible…
Part Number: TCAN1044A-Q1 Other Parts Discussed in Thread: TCAN1044AV-Q1 , TCAN1462V-Q1 [URGENT TOPIC]
Hello Team,
I had a doubt in TCAN1044 and TCAN1462 transceivers.
Is there a time limit regarding the start-up/power-down of Vcc and Vio? For example…
Other Parts Discussed in Thread: TCAN1042-Q1 , TCAN1462V-Q1 , TCAN1463-Q1
Hi Team,
Good day!
We need a CAN TRANSCEIVER part with below specification
1)CAN FD support (5 & 8Mbits) 2)VIO pin required & supply voltage level is 3.3v 3)Should have CAN…