Part Number: TCAN330 Hi,
From the datasheet of TCAN330DR, I saw the Bus dominant mode fault current would be 180mA considering the condition of CANH stuck at -12V.
I am assuming this would be arrived as below,
maximum faulty current = Faulty voltage…
Part Number: TCAN330 Other Parts Discussed in Thread: SN65HVD232 , TCAN332 Hi,
The customer has a demand for a CAN bus transceiver, which requires CAN signal input and RS signal output. Whether SN65HVD232 is the best solution?
Regards,
Charlie
Part Number: TCAN330 Hi,
Please help to provide the basic version of the CAN transceiver that conforms to the ISO11898 standard, thank you!
Regards,
Charlie
Part Number: TCAN330 Other Parts Discussed in Thread: TCAN332EVM Hi.
A question about the Test Points in CANH & CANL in TCAN330 EVM board.
The board has TPs directly connected to the CAN signals and other TPs connected to the signals through a resistor…
Part Number: TCAN330 Other Parts Discussed in Thread: SN65HVD257 , TCAN337 Hi,
I am currently using CAN transceiver "SN65HVD257" in my design for redundant multi topology CAN network.
1. Can " TCAN337" be used as an alternate ? (difference…
Part Number: THVD8000 Other Parts Discussed in Thread: TCAN330 , THVD8010 , THS6222 Tool/software: Hi team,
I have a question about THVD8000, could it work with CAN communication?
BR
Jingguo
Part Number: TCAN330 Other Parts Discussed in Thread: TCAN1043-Q1 When I use TCAN330 connected two devices,
CANL connect to GND,communication is still normal,so system can not distinguish this failure.
What can we do to distinguish this failure.
And how…
Part Number: TCAN330
Hi Champs,
as i learned, the 3.3V CAN transceivers are compatible to the ISO DIN 11898 but they are not compliant to it, right? do you see major customer concerns about that or any known issues?
This documents gives some further insight…
Part Number: TCAN330 Hi,
I have a question when using TCAN330. When I use multiple TCAN330, their CANH and CANL connect respectively, as the attachment picture. My question is, when part2 and part are not powered or there is large leakage at CANH/CANL…