Part Number: TCAN330 Hi,
I have a question when using TCAN330. When I use multiple TCAN330, their CANH and CANL connect respectively, as the attachment picture. My question is, when part2 and part are not powered or there is large leakage at CANH/CANL…
Part Number: TCAN330 Hi team,
The customer plan to use 3.3V can transceiver.
If the customer connect the 5V CAN transceiver board by mistake, the ACK signal may 4.5V.
The device would be work correctly. But one of the concern is that reverse current…
Santu,
We have a new line of 3.3V CAN transceivers releasing later this year, otherwise the TCAN330 would be a good, relatively newer replacement devices. And the CAN FD transceiver can still support CAN2.0B.
Regards,
Eric Hackett
Part Number: TCAN330
Dear Team,
My customer is surveying CAN controller and CAN transceiver solutions for their CAN device.
Here are some requirements of CAN solution:
1. 1Mbps datarate (No need CAN FD)
2. Need to support SAE J1939 spec.
Now they prefer…
Part Number: TCAN330 Hi,
In the TCAN33x a layout guideline is given, the resistors and capacitors are not defined. Can someone help me finding the correct values for these components.
This is the datasheet in chapter 13.1 you can find the layout guideline…
Part Number: SN65HVD256 Other Parts Discussed in Thread: SN65HVD230 , TCAN330 We've been using the SN65HVD256D in our 5 volt CAN bus designs, but now need a 3.3 CAN bus transceiver. When looking at potential replacements:
https://www.ti.com/interface…
Part Number: TCAN330 Hi Experts,
TCAN330 supports SOT23(3x3mm). Does TI have a plan to support more smaller package of CAN transceiver?
Regards,
Uchikoshi
Part Number: TCAN330 Hi
I am working on a canbus project for CANOPEN and J1939 protocol. My plan is to use TCAN330 for both protocol. In the datasheet, it is mentioned that it supports CAN Bus Standard such as CANopen, DeviceNet etc but does not mentioned…
Part Number: TCAN330 Hi,
My customer is wondering why for the 3.3V CAN transceiver is having different voltage level during recessive state:
For example:
TCAN330:
another part is:
I wonder if this is normal and if there are risk or things to be…