Part Number: SN65HVD232Q Other Parts Discussed in Thread: TCAN334 , TCAN332 , SN65HVD232 , TCAN330 , TCAN337 Can you please confirm SN65HVD232QDRQ1 will be used as an alternate for SN65HVD232QDR. We need same pinout and functionality. Is there any major differences…
Part Number: SN65HVD230 Other Parts Discussed in Thread: SN65HVD233 , TCAN330 , Hi,
for water meter application my customer is using
SN65HVD230D since many years, for a new design with life cycle 10years, do you still recommned this p/n or a new one?
Many…
Part Number: SN65HVD230 Other Parts Discussed in Thread: SN65HVD251 , SN65HVD233 , TCAN330 Hi, expert
My customer is using four CAN transceivers, and when the receiver node receives right signal, then output ACK. But every node will have a response difference…
Markus,
EDIT: I was incorrect, the TCAN330, TCAN332, TCAN334, and TCAN337 devices come in the SOT-23 package, which is smaller than the SOIC8 package.
Regards,
Part Number: TCAN330G Other Parts Discussed in Thread: TCAN330 Hi,
I want to know what is difference between TCAN330 and 330G.
According to the Device comparison matrix TCAN330 has 1Mbps of DERATE and 330G has 5Mbps of DERATE.
Can I know what DERATE mean…
Part Number: TCAN330G Other Parts Discussed in Thread: TCAN330 Hi Team,
My customers are using TCAN330G.
On the system, it may be opposed to the CAN transceiver of the original competitor(PCA82C251T).
Can it communicate?
Best Regards,
Kenji
Part Number: SN65HVD256 Other Parts Discussed in Thread: TCAN337 , TCAN330 , SN65HVD234 , SN65HVD230 Hello,
Our customer use the SN65HVD256 with the VRXD as 3.3V.
The customer are considering a new project. They will use the supply voltage as only 3.3V. …
Part Number: TCAN1051V-Q1 Other Parts Discussed in Thread: TCAN330 , SN65HVD233-Q1 , TCAN1051 Hy,
we are realizing a listen-only CAN application (OBD CAN logger). We are planning to use the TCAN1051V-Q1 as physical interface.
We assume, that we do not need…
Part Number: SN65HVD232 Other Parts Discussed in Thread: SN65HVD233 , TCAN330 Hi,
a customer asked me whether the desired part SN65hvd232 would resist a +-30 volt levels transient as well as over a longer period.
These specs are off attention and I need…
Sulyn,
You may want to consider TCAN330, which has silent mode. The device has other nice features like both TX and RX dominant time out. Please let us know if you have other questions.
Regards,
Hao