Part Number: TCAN334 Tool/software: Hi Team,
I am using TCAN334 CAN Transceiver Chip which operates at 3.3VDC for one of our Application which is interfaced with Master MCU ST32H753ZIT6.
Its Operating speed is 250kbits/sec it is connected to 12Slave…
Part Number: TCAN334 Tool/software: Hoping to get get some guidance on correct grounding for a CAN Bus I have designed. The following diagram gives a high level overview of the system connectivity:
Some notes on the setup:
There are a total of 12 nodes…
Thanks for the reply! I've inserted a part of the schematic below.
The TCAN334 has no CAN bus activity, this has been measured with the oscilloscope. Once we replaced the TCAN334 with the SN65HVD230DRG it worked properly.The TCAN334 Pin 5 is not used…
Part Number: TCAN334 Other Parts Discussed in Thread: ESD2CAN24-Q1 Hello,
We’re investigating adding some additional protection on CANH and CANL to avoid damaging the TCAN334. The TVS part we’re investigating for this purpose has a typical channel…
Part Number: TCAN334 Hi
Does the CAN bus need to be impedance controlled in layout? With the following placement reference differential signal routing is not possible. Any suggestions?
Currently in my layout the D1 to J1 distance is 1 inch.
Part Number: TCAN334 Hello
The data sheet provides recommend values for R5 and R6 for the suggested layout on page 31, but does not provide recommended values or a range of values for some of the other resistors and capacitors. We were wondering if TI…
Part Number: TCAN334 Hello TI Support Team,
Good day
We are using 150 meters non-twisted,non-shielded 22 AWG Teflon wire for CAN Communication. During data transmission we are getting few bits of data frame error . We are using 100K baud rate. Next to…
Part Number: TCAN334 Hi team,
In TCAN334 datasheet, we can find the abs voltage for CANH/CANL is +-14V. The 14V here is that when VCC is powered, right? And if we connect the CANH/L to CAN bus, and don't power VCC, will the IC be damaged ?
In my customer…
Part Number: TCAN334 Other Parts Discussed in Thread: TCAN1044V Hi Team,
There is a good new that DIN TCAN & TLIN
Does TCAN334's TX & RX voltage could support 3.3V & 5V?
If not! Could you recommend suitable solution to me? THX
Part Number: TCAN334 Hello,
Could you please confirm that if STB and SHDN pins are both held high, that the TCAN334D will enter shutdown mode?
Thank you, Keith