Part Number: SN65HVD1040 Other Parts Discussed in Thread: TCAN334 , SN74AHC1G125 , TMS320F28377D Is RXD/TXD pin supporting 3.3V level from MCU like as F28377?
Regards
Brian
Part Number: TCAN334 My customer is looking for can tranceiver which is shorter delay time.
We suggested TCAN334 for their specs. They are requiring to us about max value of tPHL and tPHL.
Do you have max values about tPHL and tPHL of Driver and Receiver…
Other Parts Discussed in Thread: TM4C1231D5PM Hi
I am using TCAN334DR in my design, As in the layout example, there are passive components but their values are not specified. Please help me to get the resistor, capacitor values.
Thank you
Part Number: TCAN330G Other Parts Discussed in Thread: TCAN334 , TCAN330 Replace tcan334gdcnr with tcan330gdcnr. Without this function, 334G PIN8 is connected to GND.
Is tcan330gdcnr also connected to GND?
Part Number: SN65HVD230 Other Parts Discussed in Thread: TCAN334 , Hello, can multiple non-isolated SN65HVD230D CAN XCVRs be used with an upstream isolated CAN XCVR without any issues? I am currently experiencing an issue where there is coupled switching…
Part Number: TCAN337 Other Parts Discussed in Thread: TCAN330 , TCAN334 Hi experts,
Could the pin5 and pin8 of TCAN330/2/4/7 be tied to GND?
BR,
Gordon
Part Number: TCAN334G Other Parts Discussed in Thread: TCAN334
Hi Team,
Our customer will use TCAN334GDR for their application and would like to ask your help to review their schematic diagram before PCB fabrication. Here is the schematic diagram. There…
Part Number: TCAN4550 Other Parts Discussed in Thread: TCAN334 Hi all,
I am currently using TCAN4550 coupled with an ST controller(STM32F0) for my setup and it is working fine with around 50 nodes on the line.
Recently I have started working with STM32G0…
Clément,
Thanks for the additional information. And yes, the SN65HVD234 devices are quite old, still regularly used, but old.
The one big difference between the two that may be a show-stopper is the CAN bus absolute maximum rating (voltage at which…
Part Number: SN65HVD232Q Other Parts Discussed in Thread: TCAN334 , TCAN332 , SN65HVD232 , TCAN330 , TCAN337 Can you please confirm SN65HVD232QDRQ1 will be used as an alternate for SN65HVD232QDR. We need same pinout and functionality. Is there any major differences…