Part Number: TCAN334G Tool/software: Hello. This is seungwook han in korea.
now, We are using 3 TCAN334G with MCU and did CAN data rates test.
we successed 1~4 Mbps test, but we failed 5Mbps test.
because we are using 3 TACN334G, we tested loop-back…
Part Number: TCAN334G Other Parts Discussed in Thread: TCAN334 I want to use TCAN334G with standby & shutdown mode.
I have a question about standby & shutdown preference
After TCAN334 was standby mode(8pin is high), SHDN is high(5pin is high) =…
Part Number: TCAN334G Other Parts Discussed in Thread: TCAN334 To whom it may concern.
I'm a hardware enginner and we need AEC-Q100 & 3.3V & Low standby current(under 100uA) & CAN FD IC.
So, we are considering TCAN334G.
I want to know…
Part Number: TCAN334G Hi Ti experts,
My customer wants to use F280039C + TCAN334G to achieve 5Mbps CAN-FD function.
What is the suggested/maximum length of cable for 5Mbps or higher bit rate(8Mbps).
As shows in TCAN334G's datasheet, it is 40m cable length…
Part Number: TCAN334G Other Parts Discussed in Thread: TCAN334
Hi Team,
Our customer will use TCAN334GDR for their application and would like to ask your help to review their schematic diagram before PCB fabrication. Here is the schematic diagram. There…
Part Number: TCAN334G I have a system deployed with a customer that uses TCAN334Gs for all nodes in the bus. They had an incident where 32V was shorted somewhere it shouldn't and not-surprisingly a number of the TCAN334Gs failed, but not all of them.…
Part Number: TCAN334G Other Parts Discussed in Thread: DRV8305 , To the brilliant electrical engineers out there - could you please help troubleshoot a CAN issue I'm having on my hardware?
I have two boards that are being used to commutate a motor …
Part Number: TCAN330G Other Parts Discussed in Thread: TCAN332G , TCAN330 , TCAN337G , TCAN334G Tool/software: We are using TCAN330G is compatible with the ISO 11898 High Speed CAN.
TCAN330's datasheet tells that 'Pending the release of the updated version…
Part Number: TCAN334G Hi Team,
For our customer's application, they need the system can be woke up from standby by external wake up signal.
But after CAN entering standby mode and input a external CAN ID parameter to wake it up, the MCU can not receive…
Part Number: TCAN332G Other Parts Discussed in Thread: SN65HVD230 , TCAN334G Hello,
I am considering using TI 's CAN transceivers for our new project and have some questions regarding the compatibility between SN65HVD230 and TCAN332G.
Our application…