Marvin,
Document VisionSDK_Linux_UserGuide.pdf. , Section 2 has all the required details. Please ask more specific questions with the issue details to be able to provide next level details.
Regards Karthik
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 Hi, I am trying to debug an application in our custom board wich uses a TDA2, I use CCS only for debug, my source code is build using our tools, these are the steps I perform:
debugger = Blackhawk…
Part Number: TDA2E Hi, I would like to know if there is a document where you specify the manufacturer and models of the QSPI flash memories that you recommend or you have tested for this device.
Thanks
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 , TVP5147 Hi Team
There is good new that we could DIN our device!
RD need CVBS Decoder for TDA2!
Is there NTSC(VGA) Video Signal [CVBS+, CVBS-] to BT656(8Bits) [D0~D7, PCLK, Hsync, Vsync], and adopt…
Part Number: TDA2E Dear experts,
As they DSP&EVE core not used, so our customer want modify TDA2E memory map to increase A15 DDR space, but it failed. could you please help solve this problem? they have proposed a ticket on E2E show as blew: TDA2E…
Part Number: TDA2E HI~experts,
4AWR1243+TDA2XX,SDK :PROCESSOR_SDK_VISION_03_08_00_00,
usecase cascade_radar_object_detect,
comment these lines,the use case cann't work. why?I want to delete these lines ,and it cann't work.
delete these lines because…
Part Number: TDA2E Hi Sir,
1.
I have two projects and hope to use the same processor,
Two projects use different image sensor input interface, one is MIPI 2-Lane/4-lane and another one is Parallel (DVP) .
Could TDA2E support MIPI and DVP interface at…
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 Hi Sir,
What is the maximum image sensor resolution and frame rate that TDA2E can receive,
This project may use MIPI 2-lane or DVP interface, image data format is RAW data, Sensor frame rate is…