Part Number: TDA2E HI,TI:
I want to configure 709 format followling picture:
to our sdk code following picture:
please help us how to configure,thank you!
Part Number: TDA2EG-17 Other Parts Discussed in Thread: TDA2E Dear Sir,
U27 is TDA2EG-17, there are several pin model errors When I simulate TDA2EG -17 and DDR3 with HYperlynx. Please check following errors and give me suggestion.
No IC output on selected…
Part Number: TDA2E Hi Expert,
TDA3x, TDA2Px and TDA2Ex support CSI2 input.
But in VisionSDK_SW_Architecture_Details.pdf (PROCESSOR_SDK_VISION_03_08_00_00\vision_sdk\docs\Architecture)
What does it mean that "ISS Capture Only in TDA3x "
T…
Part Number: TDA2E TDA3EX EMIF is 32bit DDR3, because there is no 32bit width DDR3, so we want to connect two 256MB 16bit DDR3 to increase the width to 32bit. What's the maximum memory the TAD3EX can access? 256 or 512MB. DDR3 SPEC is as below,MT41K128M16…
Hi,
You can refer to TRM Ch 28 PWM which has eCAP to capture input signal.
However, you have to check if EVM has exposed any pin which is routed to eCAP.
https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/linux/Foundational_Components…
Part Number: TDA2E
Tool/software: TI C/C++ Compiler
Hi
I tried to modified ti_components\algorithms\REL.TIDL.01.02.00.00\modules\ti_dl\algo\src\tidl_detectionOutput.c code, but I cannot build it.
I copy ti_dl\algo folder from REL.TIDLSRC.01.02.00.00.bin…
Part Number: TDA2EG-17 Other Parts Discussed in Thread: TDA2E , DRA71 , PMP Which version of QNX is proposal to use to develop tda2e now?
At present, qnx6.6 has the BSP package of tda2e, and qnx7.0 has the BSP package of tda2x.
Can we develop and transplant…
Part Number: TDA2E Hi, team:
Customer wants to develop their own GPU profiling tool, and use PVRScope as reference.
So, where can we find the source code of PVRScope?
Many thanks.
Part Number: TDA2E The current GPU processes images with 1280*720 resolution. If the DVR function is not enabled, the average processing time of 25 frames within one second is about 30ms. If the DVR is turned on, the average time will change to about…
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 I am confused of the sparse model and dense model, I trained an sparse model and import it by TIDL, BUT NOT SPEED UP.
1. import config:
# Default - 0 randParams = 0
# 0: Caffe, 1: TensorFlow, Default…