Part Number: TDA4AH-Q1 Hello,
I have a couple of questions about TDA4AH.
(1) There are 4 part numbers, are they sharing the same package and pin out? Are they all in production now?
XTDA4AHXXXGAALY
XTDA4APXXXGAALY
XTDA4VHXXXGAALY
XTDA4VPXXXGAALY…
Part Number: TDA4AH-Q1 Tool/software: Hi TI, We have a custom board with TDA4AH-Q1 HS SoC and we are trying to boot in XSPI (Mode OCTAL-DTR (8D-8D-8D) at 25 MHz, Pin Cmd 0x0B Read Command, SFDP Disabled).
I need to better understand the low level…
Hi Ajay,
Ajay Jose said: since the AR0341 sensor cannot control the analog gain from the host side, I am adjusting only the exposure time.
That looks like a limitation of AR0341.
Ajay Jose said: However, I am encountering an issue where the output…
Part Number: TDA4AH-Q1 Tool/software: Hello TI,
We are using 9.2 SDK and fusion 1 board (FPD link III).
I would like to know we should be able to run the Onsemi's AR0233 sensor in the Single cam default demo application with 60 FPS? If so, please…
(Hi,
Scott Brown said: We have used ENET-EXP-2 for USXGMII, which is either SGMII7/8. However according to SPRSP79B isn’t USXGMII compatible.
Yes, Port-7/8 are not compatible for USXGMII. Only Port-1, Port-2 supports USXGMII/XFI interface as mentioned…
Part Number: TDA4AH-Q1
Tool/software:
Hello TI,
Could you please provide the actual encoding of the LTSSM_STATE field of the LINKSTATUS register ?
I have a gen3x2 link up and active (TDA4AH is the RC, PCIe instance 0), but the LTSSM_STATE…
Part Number: TDA4AH-Q1 Other Parts Discussed in Thread: TDA4VH Tool/software: When running our proprietary OS on TDA4AH/TDA4VH, CPU exception often occurs. The value of Exception Syndrome Register (ESR) is 0xBF000002, I recognized that the reason of CPU…
Part Number: TDA4AH-Q1 Tool/software: Hello,
After trying to implement a 10G USXGMII link in MAC2MAC on SerDes 2 (in a multilink configuration with an SGMII refclk @100MHz with internal_refclk1 and USXGMII with an external refclk @ 156.25MHz), I spotted…
Part Number: TDA4AH-Q1 Tool/software: Hi Team,
I want to save a PNG image using the single-camera app on SDK 9.2.5 (QNX). For this, I am using the function:
vx_status tivx_utils_save_vximage_to_pngfile(char *filename, vx_image image);
The function…
Hi,
AB said: Could we use the PCIe0 Lane2 and Lane3 , instead of PCIe2 Lane0 and Lane1 , to be compatible with the configuration explained above ?
Let me check with our PCIe expert whether we can use Lane2, Lane3 without Lane0, Lane1.
AB said: and…