Other Parts Discussed in Thread: TDC1011 , TDC1000 Hello,
I have a simple question. Does the TDC1011 require 2 sensors, one for TX and one for RX ? Or it is able to drive one single transducer for both TX/RX ? If latter, how does it switch between TX/RX…
Other Parts Discussed in Thread: TDC1011 , TDC1000 Hi All,
Being a novice, I'm a bit confused about TDC1011 current consumption. First page of the datasheet says operating current is 1.8uA (2SPS) where as sixth page of datahseet stays supply current requirement…
Other Parts Discussed in Thread: TDC1011 , TDC1000 , CC2650 Hi,
I am trying to connect TDC1011 to the SmartRF06EB through SPI. So, where can i connect it and how to read/write TDC1011 register values using SPI ?
Other Parts Discussed in Thread: TDC1011 To whom it may concern.
Customer is evaluating with TDC1011 for proximity sensing.
The target distance about 1.5m.
We know PGA450 is suitable for proximity sensing.
Our customer prefer to use TDC1011 because Iq…
Other Parts Discussed in Thread: TDC1011 Dear all.
Our customer is testing by EVM now. However, the measurment distance is less than 1.5 m.
Do you have any data of TDC1011 mesurment distance? Are we able to add an amplifier and increase the distance?
Regards…
Other Parts Discussed in Thread: TDC1000 , TDC7200 How to choose the number of stop pulses in level sensing and what will be the effect of choosing different number of stop pulses on level sensing?
What is the effect of different number of Tx pulses on…
Other Parts Discussed in Thread: TDC1000 , TDC1011 Hello, I am working on a fluid level sensing project. I saw introductory videos of TDC1000 and TDC1011. Transducers used in videos were quite expensive and are of 1MHz. My question is whether these TDC…
Hi Kuldeep,
Since the MSP430FR6047 can only support frequencies down to 133kHz, this solution is not going to work for you.
There are other TI options for this application. Have you looked at the TDC1011 single channel Ultrasonic AFE, https://www.ti.com…
Part Number: TDC1000-C2000EVM Other Parts Discussed in Thread: TDC1000 , TDC1011 , , PGA460 , TUSS4470 Hi
Please, can you give us your opinion for the following usecase? We tried using the TDC1011/TDC1000, but it didn't work...
Please let me know if there…
Hi Gabriel,
We do have a 10k pull-up on INTB.
I looked at the thread that you sent and in that case the problem seems to be that the TDC7200 is sending the TRIG, and consequently getting the START, before the TDC7200 SPI-CS# is asserted back high, which…