Part Number: TFP410-EP
For above RST, how long I have to wait before making ISEL/RST low again because I am using hard-wired boot strap configuration, I do not need any I2C configuration ?
Part Number: TFP410-EP Other Parts Discussed in Thread: TFP410 We have had two DVI chips (the TFP410) that have not worked. One was on initial power up and another was after testing for a while. I suspect it is the setting we have on VREF but the datasheet…
Part Number: TFP410-EP Other Parts Discussed in Thread: TFP410 What is the use of I2C pin ?
TFP410 doesn't require configuration/initialization (through I2C) unless we want to enable the DE generator
What exactly is DE generator ?
Part Number: TFP410-EP Other Parts Discussed in Thread: TFP410 , There was a previous thread entitled "TFP410 EMI-problems (radiated emission up to 1GHz)" that shows resolved, but I cannot find the solution for it. The reply to the thread from…
Part Number: TFP410-EP Other Parts Discussed in Thread: TFP410 Hi,
I am using TFP410-EP serializer for RGB to DVI. Do I need to register at HDMI.org or any other similar websites in order to procure the IC?
Thanks,
Regards,
Pruthvi
Part Number: TFP410-EP Other Parts Discussed in Thread: TFP410 Hello,
I'm in the process of filling the following information in the Linux kernel device tree:
- hfront-porch, hback-porch, hsync-len: horizontal display timing parameters in pixels vfront…
Part Number: TFP410-EP Other Parts Discussed in Thread: TFP410 Hi TI pals
We finished the SMT build 2 days ago, and we have 24 bits DRGB input to TFP410.
How do we confirm that the data has transformed to HDMI without I2C control directly?
The design review…
Part Number: TFP410-EP Other Parts Discussed in Thread: TFP410 The TFP410-EP datasheet lists a jitter tolerance on the IDCK input of 2 ns (typical), and a DVI output clock jitter max of 150-190 ps @165MHz, with a Note 4 saying the jitter is relative to…
Part Number: TFP410-EP I am trying to find out what the lead finish is for the TFP410-EP (-55 to +125C) part?
The 0-70C part datasheet shows this to be CU NIPDAU. How can I verify it is the same for the Mil temp range part?
We want to make sure it is not…
Part Number: TFP410-EP Other Parts Discussed in Thread: TFP410 Hi TI pals
Please help to design review, the schematic had sent via email to Joel.
This new post will continue until both schematic and layout finished