Part Number: THVD8000 Other Parts Discussed in Thread: TCAN330 , THVD8010 , THS6222 Tool/software: Hi team,
I have a question about THVD8000, could it work with CAN communication?
BR
Jingguo
Part Number: THVD8000 Tool/software: Hi,
I was wondering if I had 500Khz carrier frequency and a baud rate of 9600, would I be able to pass EN55032 Conducted Emissions?
Part Number: THVD8000 Tool/software: Hi experts,
May I know what's the reason we recommend to use 2Mohm for MODE? What would be acceptable range or any concern what if changing to other value?
Thanks,
Allan
Part Number: THVD8000 Other Parts Discussed in Thread: THS6222 Tool/software: Hi Team,
We want to design Power line communication system for DC rectifier. Our system voltage will be from 48V to 60V. with module of ~100. Can we develop by Using THVD8000…
Part Number: THVD8000 Tool/software: Hi There.
I am searching for the solution for RS485 with power delivery.
More specifically, I need to use 3 -wires to carry the data and power at the same time.
I found THVD8000 could carry RS485 on power, but…
Part Number: THVD8000 Other Parts Discussed in Thread: THVD8010 , , THS6222 Tool/software: Hi Parker,
thank you very much for the detailed answer.
Let's keep the system with a main Central Unit and the 30 thermostats as an example.
Can I connect…
Part Number: THVD8000EVM Other Parts Discussed in Thread: THVD8000 Tool/software: Hello expert,
To follow my previous questions.
If 36V line is DC power supply not AC power supply, can the tranfermer still be used? are there difference on design for…
Part Number: THVD8000
With the THVD8000 transceiver, what should be the observed behavior for bus contention? Are the observations deterministic for all combinations of dominant and recessive bit collisions?
Part Number: THVD8000 Tool/software: Hi,
One of my customers is using the THVD8000 transceivers, sending data constantly at 115200bps (transmitting over 32V power lines), The CAN did not work until they inserted a 10ms delay between transmissions…