Part Number: CC1312R7 Hello,
My team are evaluating the use of the CC1312R7 to work as a wireless controller to DALI connected lights.
I came across TIDM-MS-DALI reference design and the was wondering if it is possible to configure the onboard peripherals…
Hello Alex,
I see you are interested in touchpad development and our MSP430FR2633. Let me try to help answer your questions.
First, in case you haven't seen our Captivate Technology Design Guide , you will find most all the information you need regarding…
Hi Nomikos,
If you want to calculate the meter constant for multiple points yourself. In excel, you can construct a plot of Expected VFR (y) vs Mean VFR (x), and use a trendline to make a linear fit.
See this thread for an example: https://e2e.ti.com/support…
Hello David,
The provided range of AVss-1 to AVcc seems to be contradicted by note 2 under section 8.7.7.4. This states that the full-scale range is given by:
VFSR- = -VREF/GAIN
Table 8.7.7.3 states that VFSR can be between 1 and 1.5 VDC. That seems…
Part Number: TIDM-3PHMTR-TAMP-ESD Hello Team,
To protect ADC pins of MCU, clamping diodes are essential. If the input voltage of an ADC pins is maximum of let us say, 3.6V, the clamping diode of 0.2V to 0.3V should be used when the diode is connected…
Part Number: MSP-EXP430F5529LP Other Parts Discussed in Thread: MSP430FR2633 , , CAPTIVATE-PGMR , TIDA-00343 , TIDM-1021 Hi team,
I am working on MSP430FR2633 MCU on a custom board using the debugger built in the MSP-EXP430F5529LP launchpad running in self capacitance…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: MSP-EXP430FR6989
Hi all,
I tried to test firmware TIDM-3LC-WATERMTR with kit MSP-EXP430FR6989. But when i tried to test, the signal from ESICH0, ESICH1, ESICH2 was very strange. I use coil 100uH…
Hi Serkan,
For IrDA, we have various code examples implemented for you to take a look at on https://dev.ti.com/tirex/explore/node?node=AL1cTv9MtErSpQwUL56jsQ__IOGqZri__LATEST
These examples can be found in the MSP-EXP430G2 , MSP-EXP430G2ET , and MSP-EX…
Hello Dennis,
the water meter is a DN20, we have the same problem with a DN15, we are using LPH.
You can see the problem was the same 2 years ago, but the tips from this post doesn't work anymore
TIDM-1019: USS - Meter constant error - MSP low-power…