Part Number: TIOL1113 Other Parts Discussed in Thread: TIDA-010016 , TIOL111 , TIOL1123 , TIOL221 Could you please just check and clarify that, a TIOL113 chipset is IEC 61131-9 complaint or not?
If yes, then can share more details on that ( e.g. which…
Part Number: TIOL111 Hi team, There is a difference in the way the current flows TIOL111 and TIOL1113 at CQpin, so I'd like to know if this is normal operation. TIOL111 : 2A TIOL1113 : 0.3A Is it possible that TIOL111 is broken? If so, what are the possible…
Part Number: TIOL1113 Hi,
I am working with the PIC32MM0256GPM048-I µC, which is connected to the TIOL111-3.
My problem is that the output is in NPN instead of PNP.
The output EN of my µC (pin 38 alias RD0) is connected with a simple wire to the…
Part Number: TIOL1113 I am currently programming an interface for a device (slave) with a connected sensor to make it ready for the communication with a master device via IO-Link.
In my scenario I use the TIOL1113 transceiver for data communication…
Part Number: TIOL1113 Other Parts Discussed in Thread: TIOL111 Hi sir,
Do you have any demo of TI that implements the host based on TIOL1113as the IO-link interface? Related IO-link protocols. The chip TIOL1113 is used in my design, and the host is…
Part Number: TIOL1113 Hi team,
Could you please share the temp drift(temp coefficient) data, especially its histogram and std.dev for the integrated LDO of TIOL1113? I would like to also confirm followings.
- over operating free-air temperature range…
Part Number: TIOL1113 Hi Team,
can you help with the question below:
currently we are in the development of an IO-Link product again at the safety consideration. We would use the TIOL1113. The question is, if the 60V is present at pin L+ or CQ in…
Part Number: TIOL1113 Hello,
I want to use the TIOL1113 at Ta = -40 .. +85°C. Io (lim) = 150mA. Io (nom) = 100mA. I have 2 questions regarding inductive loads:
1.) Figure 29 and 30 of the datasheet show that the internal circuit can demagnetize the…
Part Number: TIOL1113 Hello team,
I have a question regarding the TIOL1113: In particular I have a question about the Wakeup signal generated by the TIOL when the Master intends to activate the IO-Link communication. From datasheet I infer that the…
Part Number: TIOL1113 Other Parts Discussed in Thread: MSP430F6726A Hi,
In order to comply with COM3, how many baud rates of the communication UART with the MCU are required?
The MCU is MSP430F6726A, and BRCLK = 8MHz is assumed.
Best Regards,