Part Number: TL16C752B-EP Other Parts Discussed in Thread: TMS320F28377D Tool/software: Code Composer Studio Hello Guys,
I am using 3 TL16C752B with TMS320F28377D and getting some problem with EMIF Interface with TL16C752B
Error symptom
- We manufactured…
Part Number: TL16C752B-EP Dear All,
We are looking for Alternate part to TL16C752BPT Dual UART from TI. i found two equivalent parts from TI web, from one of the TI rep assigned to me is not yet confirmed those are alternate part & Availability for next…
Part Number: TL16C752B-EP Hi Team, Our customer needs to identify the ESD classification of TL16C752B-EP. Do we have data on its ESD level, particularly the HBM? Thanks in advance! Kind Regards, Jejomar
Part Number: TL16C752B-EP Hi team,
about EP grade limited to 110°C max ambient:
RTHJA is 61°C/W, Tj max 150°C.
Delta T(J-A) = worst case 61°C/W * 0.020A* 3.3V = 4°C increase max => Tj max 129°C @ Ta 125°C => lower than 150°C Tj max.…
Part Number: TL16C752B-EP Hi, team.
Could you please let me know about "required delay" on baudrate.
Compare with TL16C752B(SLLS405C), TL16C752B(SLLS405A) and TL16C752-EP(SGLS153B), required delay time on 115kbps is different.
I guess 0.5us is…
Part Number: TL16C752B-EP Hi there, I'm trying to get a TL16C752 DUART to work with an RM57 microcontroller, I need to communicate at 1900baud , but I can't get the chip to work. Does anyone have any sample code (in C) for communicating with these chips…
Part Number: TL16C752B-EP Hi, to whom it may concern
I ask about TL16C752B.
We have two question, could you please answer?
Q1 ;
When the RX time-out is happened, what is the LSR[0] register value?
Is it “1” or “0”?
Q2 ;
…
Part Number: TL16C752B-EP Other Parts Discussed in Thread: TL16C550C Hi,
on Octopart you have advertisement that we can replace SC16C652BIB48 with TL16C752BTPTREP. As I checked datasheets I see that units are pin compatible, but NXP has 32 bit FIFOs and…