Avi,
The TLC59108 and TLC59108F are very similar devices. They key difference is how the output current is set. The TLC59108 are constant current outputs set by the value of the resistor to ground on the REXT pin. The TLC59108F are open-drain outputs…
Hi ELIAS VILLEGAS,
Thanks for the reply.
1) Connected STAG# to VCC_3.3V through 10K resistor.
2) Pulled down CLKSEL to ground through 1K resistor.
I used NXP "PCA9633DP1" IC as Back-light controller.
Is there any IC from TI, which suitable…
Hello Nicola,
You are correct, the thermal information is not part of this document. With the next review of the datasheet we plan to add this information.
Please check the TLC59108F datasheet for the thermal impedance data for the 2 packages. The part…
Julia,
I'd like to make sure I understand a few things. If I'm mistaken, please clarify.
You are using a single TLC59108. It is not a TLC59108F (open drain version) as evidenced by register 0x13.
When you refer to each string, it is one string…