Part Number: TLIN1431-Q1 Other Parts Discussed in Thread: TLIN1441-Q1 Tool/software: Hello,
First of all, i would like to know the difference in the safety features between TLIN1441-Q1 and TLIN1431-Q1.
However, the device TLIN1431-Q1, has the safety…
Part Number: TLIN1441-Q1 Other Parts Discussed in Thread: TLIN1028-Q1 , TLIN1431-Q1 Hi Expert,
I have some questions about wake up requirement in standby mode.
Firstly, in customer's use-case, there have some wake up detection requirements on MCU…
Lynn,
The TLIN1441-Q1 uses the same oscillator in pin and SPI modes. The electrical characteristics show a wider range that, when designing to, will ensure design robustness. This is why you might see some wider ranges on max/min values in the electrical…
Part Number: TLIN1441-Q1
hi team
please confirm if the chip will enter sleep mode and shut down Vcc ( which means no Vcc output if Vcc overvoltage detected) once the Vcc overvoltage occurs
from p30 state diagram, I can see the LDO off during…
Part Number: TLIN1441-Q1 Hi Team, Our customer raised a concern about a discrepancy on pins RXD and TXD on pages 41 & 42 of the TLIN1441-Q1 datasheet. The Pin Configurations section of the datasheet shows RXD and TXD pins to be pins 10 & 11 respectively…
Part Number: TLIN1441-Q1 Hi Expert,
Considering the functional safety requirement, customer have some questions when using TLIN1441-Q1 watchdog function.
The background is that customer use the pin mode for watchdog and choose the 40ms twindow(WDT…
Part Number: TLIN1441-Q1 Hi team,
I got below questions from customer on TLIN1441-Q1. Would you pls help check?
1. Do we have any distribution of Vcc voltage and OV threshold? Because the OV threshold is 5.6V typ and 6V max, however customer use Vcc…
Part Number: TLIN1441-Q1
Dear experts,
As we all kown, LDO outputs voltage not starting from 5V. And 1441 will check which mode to enter when Vsup >=UVsup, Vcc > UVcc.
When VCC is increase very slowly at power on or at UVcc event recovery, and our…