Part Number: TLIN1441-Q1 Other Parts Discussed in Thread: TLIN2441-Q1 One of out customers is considering using TLIN1441-Q1 for their new products.
The products are not automotive product. Also the power supply voltage in the product is 24V.
They have…
Shinji,
Shinji Tsuji said: When it is configured as nWDR, it is Open drain output and internally pulled up to Vcc=3.3V, correct?
That is correct.
Shinji Tsuji said: How much is the minimum VOH?
There technically is no minimum VOH, since you can pull it…
Part Number: TLIN1441-Q1 Hello guys,
One of my customers is going to evaluate TLIN1441 for their new products.
Also they are looking for TI TVS device to protect LIN bus line of this device from surge and ESD.
Could you tell me any TI TVS device if you…
Part Number: TLIN1441-Q1 Hi
1. Can LIMP, nRST and WAKE pins be suspended without use?
2. WDT grounding, how long will the NWDR reset after the feeding stop?
3. Can the PIN/NCS PIN be directly grounded?
4. Is there any application hint for tlin1441-q1…
Part Number: TLIN1441-Q1 Dear TI,
Below is the latest schematic of TLIN14415-Q1 and I want to use it in PIN mode, will you please review the schematic, thank you!
Another question, I do WCA for TLIN1441 and the temperature will be 139°C at 85°C ambient…
Part Number: TLIN1028-Q1 Other Parts Discussed in Thread: TLIN2441-Q1 , TLIN1441-Q1 Hey Team,
I have two questions and would appreciate your help in answering them.
1. I am wondering if the TLIN1028-Q1 have overvoltage protection on the Vcc line. I am not…