Part Number: TLK10022 Tool/software:
Hi Team,
Does TI intend to continue supporting and producing the device? I see that there is no revision update after 2013.
Additionally, I’m interested in purchasing the TLK10022 eval board, but I noticed that…
Part Number: TLK10022 We would like to setup a BER test using loop backs connecting HS TX transmitting PRBS pattern to HS RX inputs and monitoring for bit errors detected.
Is there a way to understand what the EVM GUI is doing so we can replicate it…
Part Number: TLK10022 BER-test configuration.docx
Hi,
I use TLK10022 EVM board and GUI for BER testing, the config is discribe in the document, please help to check why the result is NAN and how to config, thanks.
Part Number: TLK10022 Hi,
Is it fair to say if we only use the TX side of the chip (aggregator only) then power consumption will be cut in half, 0.95W instead of 1.9W?
and if we run it at lower speed than 10Gbps would the power be almost cut accordingly…
Part Number: TLK10022 Hello everyone,
Using LNK10022, I want to aggregate bunch of "4 low speed streams each at 1.8Gbps" and make "faster data streams at 7.2Gbps".
Based on below calculation I can use a REF CLK between [150-360] MHz.
According…
Part Number: TLK10022 Hi Team,
Is there an available RTL code available for this device? Can you please share?
If none, can you please help create?
Thanks in advance.
Regards,
Marvin
Part Number: TLK10022 I have trouble to order TLK10022EVM from TI website. The request button at https://www.ti.com/tool/TLK10022EVM#order-start-development is not valid any more.
Thanks,
Frank
Part Number: TLK10022 Other Parts Discussed in Thread: TXB0108 , LSF0204D Hi,
I am going to manage 8 TLK10022 chips over a common 3V3 MDC/MDIO bus.
Could you suggest a voltage translator/ buffer (3V3 to 1V8), with partial power down mode feature,…