Part Number: TLK10022 We would like to setup a BER test using loop backs connecting HS TX transmitting PRBS pattern to HS RX inputs and monitoring for bit errors detected.
Is there a way to understand what the EVM GUI is doing so we can replicate it in…
Part Number: TLK10022 I have trouble to order TLK10022EVM from TI website. The request button at https://www.ti.com/tool/TLK10022EVM#order-start-development is not valid any more.
Thanks,
Frank
Part Number: TLK10022 Hi Team,
Is there an available RTL code available for this device? Can you please share?
If none, can you please help create?
Thanks in advance.
Regards,
Marvin
Part Number: TLK10022 Other Parts Discussed in Thread: TLK1501 , , TLK10081
I am planning the setup as shown and the communication will actually be both Tx and Rx between the TLK1501/TLK10022/FPGA. This setup will be repeated 16 times with the same FPGA…
Hi, Drew
Please show me your BER testing page.
When I config that you mentioned above, the BER is not NAN ,but it's always ERROR because error counter is growing. Does this mean the function of TLK10022 is wrong? How to get Error Counter 0 or loopback…
Part Number: TLK10022 Hello all,
For a design in which an aggregation is made from 5 to 10Gbps I am using a TLK10022. I will be using channel A input 0 and 1 (INA0P/N INA1P/N) as the inputs and at the output the HSTXAP/N pins (in 2:1 mode) .
I was wondering…
Part Number: TLK10022 Hi team,
support need!
The customer finds that there is a path inputting in LS and outputting from LS drawn in green path. So customer wonders to know how to set register to achieve input in LS and output in LS without via HS. …
Part Number: TLK10022 Hi,
Is it fair to say if we only use the TX side of the chip (aggregator only) then power consumption will be cut in half, 0.95W instead of 1.9W?
and if we run it at lower speed than 10Gbps would the power be almost cut accordingly…
Part Number: TLK10022 Other Parts Discussed in Thread: TXB0108 , LSF0204D Hi,
I am going to manage 8 TLK10022 chips over a common 3V3 MDC/MDIO bus.
Could you suggest a voltage translator/ buffer (3V3 to 1V8), with partial power down mode feature, meaning…