Hi Shengyue,
I understand and see the issue. Has testing been performed with any other values for HS_SERDES_CONTROL_3? Or has testing only been performed with 0xd400?
Best,
Lucas
Part Number: TLK10031 Other Parts Discussed in Thread: DS110DF111 Hi, I want to use TLK10031 to interface it with NVIDIA JETSON AGX ORIN which is having XFI interface so can we use TLK10031 to interface XFI (ORIN) to 10Gbase-KR (Backplane) application…
Part Number: TLK10031 Hi,
I have a customer want to do high-speed parallel series, high-speed data storage function, want to choose this type of product, please recommend the main product?
Thanks~
Part Number: TLK10031 Hi,
In order to verify the performance of TLK10031 data paths on our board, please your support with 10GBASE-KR eye mask or mask defintions.
Thanks,
Roy Roif
Other Parts Discussed in Thread: TLK10031 Hi expert
we use the tlk10031 for 10G-BASE-R funciton.( #disable auto-negotiation;#turn off lt_training )
in our normal test, we find the TLK10031 HS_ERRRO_CNT in not zero. But in our xgmac , we can not find the crc errros…
Part Number: TLK10031 Hi
Now we have a TLK10031 connecting to a 10BASE-R SFP device
We test the Deep Remote Loopback mode and find the status PMA/PCS receive link up ; but PMA/PCS fault condition is detected on tx path , so our connecting point ( 10BASE…
Part Number: TLK10031 Hi,
I have difficulties on getting link with PC.
My design is as following:
In order to get link is it enough to supply power and clk ? Or should I configure the tlk10031 with specific configuration?
I configured the TLK as…
Part Number: TLK10031 Our setup for the TLK10031 is
Ref clock = 156.25MHz
- LS side: connected to 4 channels XAUI
HS side: connected to Xilinx FPGA via backplane.
Please advise how to configure TLK10031 to 10-KR mode with Auto Negotiation disable.
Thank…