Hi Adrian,
Adrian Nicolau said: Please correct me if I'm wrong, but I would have expected that even without any additional configuration to still get to PLL locked
I believe you are correct. I had incorrectly assumed that this was more similar to a…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232 TLK10031_LS.pdf
our system is as attachment pdf. our TLK10031 config is as follows:
global reset"
"0x8610" > "0x401E0000"
#disable auto-negotiation
"0x2000" >…
Part Number: TLK10031 Hello,
How to know the data activity status in TLK10031. When data transfer is happening through TLK, I wants blink a LED. So how to find data transfer is happening via TLK. Is there any register or pin which shows the activity of…
Part Number: TLK10031 Hello,
I am using TLK10031 in 10G-KR mode for my project. TLK10031 is working fine in 10G-KR mode. Now I wants change the TLK data rate to different speeds like 1536 Mbps, 3072Mbps, 6144 Mbps, etc. Can you please suggest me a method…
Part Number: TLK10031 Hi Sir,
We are using TLK10031 chipsets in our board. Once we Powered ON the board, we have checked the voltages for 1V & 1.8V. The 1V & 1.8V are within the range as per specified in the datasheet.
The TLK10031 is heating…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232 , TM4C129DNCPDT Hi
We are implementing 10G repeater application using 2 number of TLK10031 PHY transceivers.
Please find the attached block diagram for the application.
As per application…
Hi Rodrigo Natal,
Our issue is resolved, we are able achieve the link successfully. With previous settings we disabled PRBSEN pin, so our device got proper link with HS and LS errors as 0.
But we have one doubt, we have a Link/Activity LED on our board…
Part Number: TLK10031 Greetings for the Day,
We are facing issues in accessing few registers of TLK10031(Specifically Vendor Specific registers)
We are using TM4CDNCPDT microcontroller with TLK10031 transceiver for 10G repeater application. We are implementing…
Part Number: TLK10031 We designed a circuit with the TLK10031 PHY that will be used for a VPX Ultra-thin Pipe, thus we will use 1G-KX mode only. Can the TLK10031 be configured to operate in 1G-KX mode only, but still support auto negotiation? The idea…
Part Number: TLK10031 Customer has an FPGA with a 10BASE-KR output but would like to convert this to 10GBASE-T copper. Could the TLK10031 help in this conversion by interfacing to the FPGA over -KR data link and then connect to -T PHY using XAUI? Block…